Part Number: TPS3704-Q1 Hi Expert,
Our customer want to develop a power solution with ASIL-B. For purely discrete solution, we may need a voltage supervisor with ASIL-B level. As I learn, we only have TPS3704-Q1 with very limited voltage option. Our customer…
Hi, Walter
Thanks for your reply.
- We have separate power supply for TPS3704-Q1 , so, we don't use debugger power supply to power TPS3704-Q1 .
- We are using TI TMDSEMU110 debugger to program our microcontroller.
-Our main question is, if we have the above…
Part Number: TPS3704-Q1 Hi Team,
Regarding the TPS37044 options, I can't find the whole PN info in the datasheet. The datasheet doesn't show the detection with option Bx. Can you please explain the difference between the PNs?
Thank you, Delan…
Part Number: TPS3704-Q1 Hi expert,
My customer is choosing a supervisor for F28377D.
They found TPS37042 is good for them. But they still have two questions:
Question1. we have many choice listed on datasheet, this is what they want to choose:
but I…
Part Number: TPS3704-Q1 Hi,
We can find "TOL : Tolerance Programming Range" on the datasheet P.7. What does this mean?
Could you please let us know the parameter of TOL "Tolerance Programming Range"? Please advise us.
Thanks and best…
Part Number: TPS3704 Hi,
We are thinking of replacing ADI's LTC2914 with TPS3704.
Q1. Please tell me about the SENSE1-4 pins of TPS3704. Can the TPS3704 detect the upper limit (3.3V+10%) and lower limit (3.3V-10%) separately? The LTC2914 has separate…
Part Number: TPS3704
Dear team,
I know TPS3704 is Functional Safety-Compliant device. so we can see function safety information at ti.com.
Is the function safety data of TPS3704 same with TPS3704-Q1 data?
If not, How can I get full FMEDA data for TPS3704…
Archie,
You could use a diode with pull-up resistors on either side to prevent a low signal from TPS3704-Q1 from appearing on the TCAN1167-Q1. When the cathode is facing the TCAN1167-Q1, this would still allow it to pull low and pass a low output, but…
Other Parts Discussed in Thread: IWR6843AOP , TPS35-Q1 , TPS3435 , TPS3704 Hi there.
I'm dave hardware engineer.
I designed system using 28388D. I need 5ms time out watchdog ic.
Can you recommend?
Do you have it?
thank you.
(IC that resets when no pulse…