Part Number: TPS3762-Q1 Other Parts Discussed in Thread: TPS3762
Hi Team,
We promote TPS3762-Q1 to customer since they need latch function and can handle 50V rating.
I notice the datasheet mention UVbypass, not quite understand this part.
Could…
Hi Abhinav,
Thanks for your question!
My recommendation is to use the TPS3762-Q1 over and undervoltage supervisor.
https://www.ti.com/product/TPS3762-Q1
This device has a wide input voltage range (2.7V - 65V) and also has features such as built…
Part Number: TPS388C0-Q1 Other Parts Discussed in Thread: TPS3762-Q1 , TPS37100-Q1 , TPS3760-Q1 , TPS3700 Tool/software: Hi
I have some questions which I was not able to answer with the datasheet.
In the datasheet, there is a latched WDO mentioned…
Hi Nitesh,
Yes we do have supervisors that has hysteresis greater than 400mV. Please find TPS3760-Q1, TPS3762-Q1 which they both can be connected directly to 12 V / 24 V automotive battery system for continuous monitoring of over (OV) or under (UV)…
Hi Devin,
Exceeding the absolute maximum rating of 6V can cause irreversible device damage and is not recommended by TI. I would recommend swapping to a 65V capable device (able to handle both the 12V battery rail and and voltage transience).
We have…
Part Number: TL431 Other Parts Discussed in Thread: TPS3760 , TPS3762 , TLVH431 , TLV431 , Tool/software: Regarding over voltage protection above VIN 29V.
When VIN is 29V, VKA is 2V. The mosfet Q1 turn on. It has not protected.
I want to add new R320…
Hi Jesse,
Thank you for your reply.
Q1. I am reviewing the TPS3762 datasheet and noticed that the specific threshold voltage (VIT) for the "W7 ±7%" setting is not explicitly mentioned. Could you please clarify what baseline threshold voltage the …