Part Number: TPS3779-Q1 Other Parts Discussed in Thread: TPS38-Q1 , TPS37-Q1 hello :
i want to use this part to monitor power, this is functional safety project.
So, could you provide failure mode, failure rate and so on. i want to calculate FMEDA…
Part Number: TPS3779 Hello,
I am using TPS3779 part in my design for sensing 3.3V and 1.5Vdc voltages. I had used 10Kohm and 6.65Kohm voltage divider network for 3.3Vdc monitor; 6.65Kohm and 49.9Kohm divider network for 1.5Vdc monitoring with 1% tolerance…
Part Number: BQ24078 Other Parts Discussed in Thread: TPS3779 , BQ24075 Dear support team
I would like to build a battery charger incl. power path management with the BQ24078. As this chip does not feature an under-voltage protection (prevent discharging…
Part Number: TPS3779 Other Parts Discussed in Thread: TPS3780 , Hello,
My customer is considering using the TPS3779/TPS3780 in a new design. We had some questions going over the potential opportunity around the ESD diodes of the device.
Assuming that the…
Part Number: TPS3831 Other Parts Discussed in Thread: TPS3760 , TPS3779 , TPS3704 Hi,
I know the TPS3831 says that the max recommended current is 8 mA, but is the device short-circuit protected? We have an application where the RESET output is at 3.3V from…
Other Parts Discussed in Thread: TPS3779 I have a question concerning TPS3779 dual channel voltage sensor.
The datasheet defines in page 12 the VDD overdrive.
However, in graphs 16 to 19, the VDD is constant but the overdrive isnt'.
How could it be…
Part Number: TLV840 Other Parts Discussed in Thread: TPS3780 , TPS3779 , Hi Expert:
I make a long push button circuit with CD4013.
The circuit shows below
I use the /Q of second CD4013 to enable the following regulator.
I use lithium battery voltage to…