Part Number: TPS38 Hello there,
Is it legit to connect both Cap and FET to the CTRx/MR pin as shown on below snippet?
My design intent is:
When turning FET on (CTRx/MR low), the TPS38's RESET output asserts low;
When FET is turned off, the Cap…
Part Number: TPS38 Hi team, Our customer have the question described below. We got MPN TPS38A909066DYYRQ1 from custom,
From datasheet, We can match the corresponding code, but Our procurement has confirmed with TI that this MPN didn’t be found.
Please…
Part Number: TPS38 Hello Experts,
I am experiencing an issue with a circuit that uses this device, and I would appreciate your support in identifying the root cause.
I am using this device to monitor a 48 V power line. In many cases, the device becomes…
Part Number: TPS38 Tool/software: Dears,
My customer Dalian Haitian has an overvoltage monitoring requirement. The overvoltage threshold is 2.9V, reset output, push-pull and open-drain output are all available. Currently, the client wants to use TPS38J010122…
Part Number: TPS38 Hello,
We have a product uses TPS38B752933DSKR for reset control, the pin 1 - VDD is 13.8V.
I find the pin 6 - "CTR1/MR_N" hasn't external pull-high circuit.
I would like to know, does this pin 6 have an internal pull-high?
Part Number: TPS37-ADJ-CALC Other Parts Discussed in Thread: TPS38 , TPS37 Hi team,
I am FAE of OTIS.
Customer wants to use TPS37/TPS38 spice model to do some simulation.
However, they have met with two issues:
When they want to use their Cadence…
Part Number: TPS38 Tool/software: Hi team,
Customer get one request for power monitor.
They would like get 2 inputs, 1 outputs; when the all the input detect low signal, then output generate reset signal(LOW);
Could you help check if any chip could…
Part Number: TPS38 Tool/software: Hi,
We use the TPS38 to delay the power on of an external supply. To switch the supply, we use an ideal diode controller (LM74800), see figure below.
The exact PN is TPS38A0101DDDSKR, the label on the housing is 32GL…
Part Number: TPS38-Q1 Tool/software: Subject: SPICE Model Request for TPS38A010122DSK*Q1
Dear TI Support Team,
Could you please provide the SPICE model for the voltage detector TPS38A010122DSK*Q1, our project requires it for accurate simulation. …
Part Number: TPS38-Q1 Tool/software: hi there,
for a low power battery operated design, can I use OV/UV supervisor ICs to enable a dc/dc converter during OV/UV?
thanks.