Part Number: TPS3803-Q1 Customer would like to do the system thermal evaluation. Could you offer the max. TJ of below two parts? Thanks.
TPS3803-01DCKR
TPS3803-01QDCKRQ1
Regards
Brian
Part Number: TPS3803-Q1 Other Parts Discussed in Thread: TPS3808E-Q1 , TPS3890-Q1 , TPS3899-Q1 Goodmornig,
I shall power supplies the device TPS3803-01QDCKRQ1 at 1.8V.
On my schematic, the SENSE pin can go up to 6V. I would like to know if that pin…
Part Number: TPS3803-Q1 Hello,
As per the datasheet of TPS3803-Q1, the power dissipation rating is 321mW for Ta< 25 degrees C. Can you please let me know how this can be calculated theoretically?
Because, RθJA Junction-to-ambient thermal resistance…
Part Number: TPS3803-Q1 Dear team
The customer would like to know, what different about TPS3803-01MDCKREP,TPS3803-01QDCKREP and TPS3803-01QDCKRQ1.
Could you help to recommend.
TPS3803-01-EP:
TPS3803-01MDCKREP
TPS3803-01QDCKREP
TPS3803-01-Q1…
Part Number: TPS3803-Q1 Other Parts Discussed in Thread: TPS37 , TPS38 , TPS3808 , , TPS3803 Hi team,
Is there any simulation for this device?
Can this device be used to sense voltage higher than VDD such as 16V, after the resistor divider at SENSE…
Part Number: TPS3803-Q1 Hello,
We are having a special operating condition of our device, where in a NiMH battery is used. Our current application is to cut off the operation at one particular voltage, and due to the property of battery which regains…
Part Number: TPS3803-Q1 Other Parts Discussed in Thread: TPS3803 Hi Team, Could you tell me the difference between red part and blue part? I would also like to know why these part names are completely different. Best Regards, Yaita
Part Number: TPS3803-Q1 Hi team, My customer is thinking of replacing to -EP from -Q1 due to delivery issues. Is TPS3803-01-EP made using the same die as the TPS3803-01-Q1? Sincerely. Kengo.
Part Number: TPS3803-Q1 Other Parts Discussed in Thread: TPS3899
Hello team,
My customer has a question about TPS38x-Q1: How reset output behaves and how its related with monitoring voltage.
Please see the graph in the attached file. Questions are…