Part Number: TPS65070 Other Parts Discussed in Thread: OMAP-L138 , TPS3805H33 Hi Berner ,
Good day!
After a long exploration, I realized that the PMIC-TPS65070 is a better option for my application. I have few Queries on TPS65070 PMIC Hardware design, could…
Other Parts Discussed in Thread: TPS65070 , TPS3805H33 Hi,
I would like to ask a question on TPS65070.
In its datasheet slvs950d, page 71, Fig. 49,
[Sense] pin of TPS3805H33 is directly connected
to DVDD3318 pins of OMAP L138.
In its application…
Can Automotive and Enhanced Products be used as drop-in alternates for commercial parts?
I have a board with TPS3805H33 . If I can't get the exact part TPS3805H33DCKR, can I drop in TPS3805H33 Q DCKR- EP or TPS3805H33 M DCKR- EP ?
For 2, and 3, they are in the datasheet.
See Supply current section for typical and max current at 2 different voltages.
I will let our packaging engineer know about the other package related questions and he can update.
Please reference the TI datasheet…
Other Parts Discussed in Thread: TPS3807A30 , TPS3805H33 , TPS3700 Is the TPS3807A30 available with a 3.09V (or close to it) Typical VDD Negative Threshold Voltage (VDD IT–)? If so, what is the minimum ordering quantity?
The customer is looking…
Hello,
I am reading the TPS65070 data sheet (SLVS950B of 12/2009) because I plan to use TSP65070 to power Omap-L138.
As I understood from the data sheet - the output Power sequence (that includes dc-dc and LDOs) can start only with PB_IN# goes low.
…