Part Number: TPS3808 Tool/software: Hi, TPS3808 has different suffix: G33 and G25. We can put 3.3V on the VDD of TPS3808 G33. How about TPS3808 G25?
Can we put 2.5V on its VDD?
When we connect 2.5V to VDD, does MR support 3.3V level signal?
Part Number: TPS3808 Hello team,
My customer is observing a spike waveform at /RESET pin when device starts up.
However, this behavior is expected because output is undefined when VDD < 0.8V.
So, is there a new device which improves this phenomenon…
Part Number: TPS3808 Tool/software: Hi,
I encountered an issue: pin 5 (SENSE) has 1.8V, but pin 1 does not output 1.8V. Could it be that the 100k pull-down resistor R2M6 to ground needs to be removed?
Thanks!
Jeff
Part Number: TPS3808 Tool/software: Hi team,
If the VDD voltage is 3.3V, what's the recommended reset voltage? In datasheet, it should be higher than VDD, why? Can it be lower than VDD such as 1.8V?
Part Number: TPS3808 Tool/software: I am using TPS3808G01 and I see in the datasheet of Section 7.5 that the VIT threshold has a tolerance of 1% typically for TPS3808G01 part. Is 1% a 3sigma value?
I am looking for tighter tolerance & want to gauge…
Part Number: TPS3808 Tool/software: Hi Team,
I am digging into the RESET delay time accuracy for the TPS3808 when I came across another thread listing the breakdown of how the 40% accuracy variance is calculated.
E2E - TPS3808: True Accuracy of…
Part Number: TPS3808E Other Parts Discussed in Thread: TPS3808 , Tool/software: Hi team,
May I know what's the different between TPS3808E and TPS3808TPS3808E:
https://www.ti.com/lit/ds/symlink/tps3808.pdf?ts=1755654475442&ref_url=https%253A…
Part Number: TPS3808 Tool/software: We set the reset time using the CT pin of the TPS3808G50.
Please let me know what happens to the reset time if that component shorts.
* I am reviewing the FMEA related to this component.
Part Number: TPS3808 Tool/software: Hi Team,
Using TPS3808G30DBVR,
CT configuration capacitor 10uF, calculated according to the formula for about 57 seconds, but the actual test is 47 seconds. What is the reason?
Part Number: TPS3808 Tool/software: Hi,
We are currently using the TPS3808G33 supervisor IC in our design to monitor the system supply voltage. As per the datasheet, the expected behavior of the IC is as follows:
RESET assertion should occur immediately…