Part Number: TPS3808 Tool/software: Dear Sir/Madam Kindly give the Grade details (Industrial/commercial/automotive), EOL, FIT rate with respect to CL=95% , temp=55 deg C for the part number mentioned above.
Part Number: TPS3808-Q1 Other Parts Discussed in Thread: TPS3808 Tool/software:
if my sense V is around 5.8V,the reset pin will output high-low alternately,but when I add a 470nf at the sense pin,it wil ok。So,can I add a 470nf?
Part Number: TPS3808 Tool/software: Hi,
I am using the version G30 of the chip TPS3808 with a typical negative-going threshold "Vit" of 2.79V. When I check the §7.5 of the specification, I see that "Vit" has an accuracy of +/-1.5% @ 25°C and +/-1.25…
Part Number: TPS3808 Tool/software:
When I touch the FPGA_RESET_L with a bus wire, or a DVM probe, it will cause the signal to go down sharply and gradually rises up.
I probed MR_L while touching the reset_l with a wire, there is nothing on MR_L …
Part Number: TPS3808G01DBVEVM Other Parts Discussed in Thread: TPS3808-EP Tool/software: Question #1
What is the suggested substitute part number from Texas Instruments for the Onsemi PN# NCV308SN500T1G?
Question #2
The TPS3808G01MDBVTEP is to Monitor…
Part Number: TPS3808 Tool/software: Hello Sir,
We are using TPS3808G33DBVTG4 IC in our design.
We want to understand meaning of G4 which is present in last two digit in part number.
Also, we want use TPS3808G33DBVT instead of TPS3808G33DBVTG4.
Thanks …
Part Number: TPS3808 Other Parts Discussed in Thread: TPS3899 現在、電源監視ICで問題が発生しています。 監視電圧2.1Vで電源を監視しているのですが、 装置の突入電流で監視電圧が落ちてしまい(数100us程度のドロップ)、装置リセットが掛かってしまいます。 監視電圧の変更が出来ないため、 上記、"数100us程度のドロップ"を無視(マスク)したいのですが、 TI様の方で何か適切な電源監視ICが有りませんでしょうか?
Part Number: TPS3808-Q1 Hi Expert,
We found a wired phenomenon on TPS3808-Q1, need your support to check the potential reason.
Below is screenshot for TPS3808-Q1 schematic. When SENSE=730mV, we can see n_RESET=1.2V if we add a 27k pull down resistor on…
Part Number: TPS3808 Hi Team,
One of my customer is using TPS3808 for their design & they have raised the queiry related to Ct calculation formula.
As per datasheet, foprmula is given as
Now as per the formula if we use 131pF in design then reset…
Part Number: TPS3808 Hi,
We are controlling the pin MR of TPS3808 with a MOSFET. But, the leak into the transistor make the MR pin to trig because of the drop into the MR pull-up resistor. This occur only when we are testing the circuit in high temperature…