Part Number: TPS3820-Q1 Other Parts Discussed in Thread: TPS3820
Hello TI engineers:
How can I get the information about TPS3820's internal auto-reset oscillator, e.g. duty, cycle time ...
BestRegards
Part Number: TPS3820-Q1 Hello,
I have several questions regarding the TPS3820-50QPDBVRQ1 device. Could you please answer each question separately?
The schematic I am using is shown below; you may refer to it while answering the questions.
Q1) When…
Part Number: TPS3820-Q1 Hi team,
If the MCU is in debug mode and no IO pin to periodically feed the watchdog as the WDI input.
Any methods to mask the RESET signal output of TPS3820-Q1 during test mode to vorbid the trigger of reset?
BR,
Manu
Part Number: TPS3820-Q1 Tool/software: Hi,
Datasheet of TPS3820-33 specifys that /RESET asserts "td" (time delay) after rising of VDD
Is "td" also applied between rising of /MR and rising of /RESET?
Thank you
Part Number: TPS3820-Q1 Other Parts Discussed in Thread: TPS3820 Tool/software: Dear experts,
I'm trying to work with the watchdog TPS3820-Q1 and a NXP microcontroller. The circuit is shown in the figure below:
The signal WDI_UC is a GPIO from the…
Part Number: TPS3820-Q1 Other Parts Discussed in Thread: TPS3820 , SN74AUP2G34 , TPS35 Tool/software: It was not clear to me whether the transition time of the RESETn output is specified in the datasheet. I need to understand the slew rate of the RESETn…
Part Number: TPS3820-Q1 Other Parts Discussed in Thread: TPS3820 Hi ,
When the PWM signal input the WDI pin, TPS3820-33QPDBVRQ1's WDO pin keep low. That is correct?
Part Number: TPS3820-Q1 Tool/software: My customer reported an urgent issue that they found TPS3820-Q1's t tout (Watchdog time out) changed permanently after they implemented the high temperature test (100 degree).
In the below waveform, reset was triggered…
Part Number: TPS3820-Q1 Other Parts Discussed in Thread: TPS3820 Hi Team,
The figure below shows the circuit and measurement waveform of TPS3820, and the questions are as follows: 1. When the WDI pin has PWM input, the output voltage of the WDO pin…
Part Number: TPS3820-Q1 Other Parts Discussed in Thread: TPS3820 Hi,
My question is about TPS3820(non-Q1).
If DWI is fixed at High when/RESET=Low(Active), is there a problem with the device?
I think there is no problem, is this correct?
Best Regards…