Part Number: TPS3824-Q1 Hi team,
My customer is asking the function temperature. Since this device can't test the loss power that I think we can't calculate function temperature Tj. Would you please provide the report of function temperature (Tj…
Part Number: TPS3824 Hi team,
thanks your support before.
Since my customer is asking the Tj of TPS3824-50DBVR, I would like to know where can I find it. I searched datasheet and can only find Ta as below picture.
I also searched at e2e below. but this…
Part Number: TPS3824 Hi experts,
Do we have the suitable socket to the MAX6318LHUK26DX-T? I find TPS3824 has s ame function, same pinout, but only 200ms delay time . My customer selected the MAX6318LHUK26DX-T becasue of 1.6s delay time .
Customer need to…
Part Number: TPS3824-Q1 Hi TI Forum,
In the datasheet of TPS3824-33QDBVRQ1 point 5 Device Comparison Table TPS3824-xx-Q1 negative Reset: is blank, is that correct? I think the negative reset is similar to non automotive version, a push-pull output.
Thanks…
Hi Zhang,
It has been a week since the last time I replied to your thread. Again, please let me know if you have any additional questions regarding TPS3824-Q1. If there are no further questions and you were satisfied with my answers, please close the thread…
Part Number: TPS3824-Q1 Other Parts Discussed in Thread: TPS3824 Hi team,
My customer is using our TPS3824-Q1 for their WDI design and they are using our TPS3824-Q1 evm.
They don't get the correctly reset signal after the end of WDI signal. The fail…
Part Number: TPS3824
Hi,
I have some confusion regarding the operation when VCC is stable. I have tried to explain my understanding through attached media.
So as per my understanding if I want to tie my RESET(bar) pin to Logic '1' , I have to…
Part Number: TPS3824-Q1 Hi team,
I have some confuse on the choice of tps3824-q1,Since we want 2.25V vision,tps3824-q1 does not has this vision,and I do not find the same function P/N to replace it.
Pls give me some recommendation on it.
Thanks
BR
Sa…
Jai,
Sorry for the delay. I investigated the radiation susceptibility and EMI/EMC data for TPS3824 and unfortunately we do not have any data for these tests. This is not a standard test we do for our devices so I can't comment on if this is the reason…
Part Number: TPS3824TPS3824: FIT Rate input parameters
Hi all, Can someone please provide me the input parameters necessary for FIT rate calculations based on IEC 62380? for example number of transistors inside the IC, technological structure( MOS? BICMOS…