Part Number: TPS3838 Team,
My customer currently uses our 3.3V , trips at 2.93 Supervisory chip TPS3838K33DBVT.
The question is:
Can they use 3.0V device that trips on 2.64V on a 3.3V rail (and still trip at 2.64V)? TPS3838L30DBVR
Thanks!…
Part Number: TPS3838 Would you tell me the maximum junction temp(Tj max) for TPS3838L30DBVR.
My customer hope to know this value for thermal simulation.
Regards,
Part Number: TPS3838
Hi team,
My customer is supposed to employ TPS3838 and he provided a question.
What will happen when CT pin is floating? Does it(CT pin floating) output RESET even if MR is NOT reset?
I look forward to hearing back from…
Part Number: TPS3838 Other Parts Discussed in Thread: TPS3808 Hi team,
My customer would like to use TPS3838 because of its low power consumption and now they are evaluating the thermal resistance. I heard that its SON package will add roughly 20~35…
Part Number: TPS3838 Hi, Could you tell me about /MR pin and RESET signal? Is there any limitation on the input voltage slew rate to the MR pin? If the input voltage rise to /MR pin is slow, Customer is concerned that RSET signals will be unstable. Could…
Part Number: TPS3838 Hi all,
I have one question: For the TPS3838 daisy chain, if we tie the reset output of the first TPS3838 to the next TPS3838’s MR input, do we need an external pull up resistor for this signal? Can we rely on the pull up from the…
Part Number: TPS3838 Other Parts Discussed in Thread: TPS3839 Hi,
I would like to drive the out load to turn it ON & OFF . so I can use the TPS3838
Is Reset pin capable of providing 3 mA [Sourcing] in TPS3838A09 [cut off of 0.9 V] ? [Please check…
Kasuya,
The MOSFET I am referring to is in the "Reset Logic and Timer" block in the "functional block diagram" on page 5 so you can't actually see it. The push-pull version (TPS3837, TPS3836) use two internal MOSFESTs in a CMOS configuration thus…
Part Number: TPS3838-Q1 Other Parts Discussed in Thread: TPS3808-Q1 , Hi Sir,
My customer found out that TPS3838L30QDBVRQ1 is ready to EOL this year and ask that does TI have replace item that pass automotive grade too. I checked the website but it…