Hello Sila,
I have tried to simulate TPS3840 design in PSpice for TI, but i am not able to get output. I am attaching my schematic file. Could you please verify if everything is correct or if any changes are needed? If the design is correct, could you…
Part Number: TPS3840 Other Parts Discussed in Thread: TLV840 Tool/software: Hi Team,
Please help to suggest pin-to-pin solution for the below competitor.
We want to replace them but the customer requires p2p.
PST8425UR
PST8414UR
PST8330UR
c_reset_pst83_84…
Part Number: TPS3840 Other Parts Discussed in Thread: TLV840 , TPS3808 Tool/software: Hi,
We have designed a complex circuit in which we use the TPS3840PL30DBVRQ1.
After testing the circuit, it is fully functional.
In this circuit we use the MR pin to…
Part Number: TPS3840 Tool/software: Hi supporter, Recently, I have worked with TPS3840 IC for delay RESET about 3s. I noticed that when i use the device in the long time, un plug and replug the power supply, the delay time of RESET is decrease very much…
Part Number: TPS3840 Tool/software: We have an issue with this reset generator.
Below you can see the TPS3840 is always powered at a constant 3.3V. The 12V is always on, thus the 3.3V zener always works.
The MCU is at 3.3V and commands the /MR pin. When…
Part Number: TPS3840 Hello:
Please assist in conducting a review of the MC project schematic about TPS3840.
Due to the urgency of the project, we hope to receive feedback as soon as possible
Part Number: TPS3840 Hi
TPS3840 in my system have VDD drop issue durring some voltage level.
But thershold level VDD is stable, and reset output is functional.
And we don't plan to change resistor value. and the system design don't care " Vpor status…
Part Number: TPS3840 Hi,
May I know there have TPS3840PH16 device can support?
I found it in datasheet table 3. But can't find it in both PACKAGE MATERIALS INFORMATION and TI website. thanks!
Thanks!
Jeff
Part Number: TPS3840 Hi,
We have used TPS3840PL28DBVR in our custom board design. We have designed the part as mentioned below.
We have gradually decreased the input VDD (28V) to 0V and captured the output RESET performance. But during the range 18.5V…
Part Number: TPS3840-Q1 TPS3840-Q1 tSTRT + tD time is measured differently from the datasheet value.
The datasheet shows 400us as the maximum value.
When I actually measured it, it came out about 10 ms as shown below.
Please find the cause why. …