Hi Dino,
Please find my answer in below.
The relation between Maximum sourcing current (IOUT(Source)) and minimum high level output voltage (VOH( min )) :
In terms of your question on the relation between Maximum sourcing current (IOUT(Source)) and High…
Part Number: TPS3840-Q1
Hi TI-team
My customer want to know min reset time delay.
Please let me know the value when CT pin = open, 10nF, 1uF.
Also, they want to know the TYP value when the CT pin is open.
The value of the red frame above.
Best Regards…
Part Number: TPS3840-Q1 Hi TI-team
Is there a possibility that tP_HL is max and tD is min ?
Since tP_HL and tD are variations in the internal circuit of the IC, are you sure that there is a correlation in the relationship between min and max ?
My customer…
BD53E23G-M is AEC-Q100 Qualified, so the best suggestion is the automotive version of the part you recommended, TPS3840-Q1. I recommend TPS3840DL25DBVRQ1 .
Thanks, Angelina Shi
Hi Brian,
The TLV840 device is p2p with the TPS3840. Unfortunately, there is no 2.7V variant of either device. However, there are 2.8V variants of the TPS3840-Q1 and TLV840, as well as a 2.5V variant of the TPS3840-Q1. Would any of these work for the costumer…
Hi Trailokya
It seem that w e currently do not have the 1.6V option for the TLV840-Q1, this is only available with the TPS3840-Q1.
This Rohm device has a 1.6V threshold voltage so TPS3840DL16DBVRQ1 was proposed as closest alternative ,right ?
The BU4216F…
Hello Kannan,
Only devices that are listed here are released: TLV840-Q1 data sheet, product information and support | TI.com
For 0.9V, the best option is industrial grade: TLV840 | Buy TI Parts | TI.com
For 0.9V, another option is this EP device with external…
Part Number: TLV840-Q1 Other Parts Discussed in Thread: TPS3840 Hello,
The typical application circuit on the first page of the schematic of the TLV840-Q1 shows a part number of: TLV840MADL29Q1.
But the only 2.9V option that shows up in the ordering information…
Hi MJ,
Thank you for reaching out to TI. The part that you are seeking is TPS3840DL31DBVRQ1 and its datasheet can be found here:
www.ti.com/.../tps3840-q1.pdf
If you have any other questions, please do not hesitate to reach out to TI for advice.
Ben