Hi Jeno,
jeno.zhang said: The WDI pin has no input and remains low, Set0 and Set1 remain high, and the WDO pin remains high;
You stated that both SET0 and SET1 remain high, as previously stated i n order to disable the watchdog SET0 = 1 (logic level high…
Hello Kuramochi-san,
For your questions,
Kazuki Kuramochi said: Is the 50% requirement truly only from placement accuracy?
I think the recommendation for thermal pad regarding thermal dissipation should exist.
or Do you think TPS3850-Q1 won't heated up…
Part Number: TPS3850-Q1
Hello Expert,
We are considering to use TPS3850H50QDRCRQ1.
This device use DRC package but datasheet has 2 type of DRC package option as like as step cut and dimple.
Would you tell me which option is used for TPS3850H50QDRCRQ1? …
Part Number: TPS3850-Q1 Other Parts Discussed in Thread: TPS3850 Hi team,
Could you please confirm that if this IC can provide both over voltage and under voltage supervision for the single Sense input?
My understanding is that undervoltage and overvoltage…
Part Number: TPS3850-Q1 HI,
TPS3850-Q1 is not working properly, and the Reset pin is always low. The circuit diagram is shown below. Please help analyze the cause.
Thanks!
Part Number: TPS3850-Q1 Other Parts Discussed in Thread: TPS3850 Hi team,
Would like to check one question for TI TPS3850.
We would like to connect WDO of TPS3850 to NMI of SoC (DRA78x) as data sheet describes.
Due to we cannot disable NMI once it is…
Part Number: TPS3850-Q1 Other Parts Discussed in Thread: ADS7138-Q1 , TPS3435 While referring the Datasheet of the TPS3850-Q1 (watchdog) the VIL is 0.25V.
While referring Datasheet the VOL of the ADS7138-Q1 (ADC) GPIO pins is 0.2 x AVDD (since AVDD…
Part Number: TPS3850-Q1
The above shown image is operating characteristics of TPS3850-Q1:
Am a bit confused with the VIL and VIH from the datasheet. Its given as 0.25 and VIH is 0.8 the VOL of MCU is 0.45, so this will impact our design. Is these figures…
Part Number: TPS3850
Hi
Im using latching watchdog timer with TPS3850 to disable LDO circuit.
First either 12V power1 or 12Vpower2 can enable the LDO. Once the MCU is powered ON with 3.3V, it will send the pulse to watchdog timer.
The watchdog timer will…