Part Number: TPS3850-Q1 If we short \RST to WDO and use a pullup (since theyre both open drain).
, and use a latching scheme as in 3430 datasheet, will we also be able to latch from both WDO or sense?
Part Number: TPS3850-Q1 Hi,
When we use the chip TPS3850H33QDRCRQ1, it will not reset without feeding the dog. What may be the problem? The schematic diagram is shown in the following figure.
Thanks!
Part Number: TPS3850-Q1
Hello Expert,
We are considering to use TPS3850H50QDRCRQ1.
This device use DRC package but datasheet has 2 type of DRC package option as like as step cut and dimple.
Would you tell me which option is used for TPS3850H50QDRCRQ1? …
Part Number: TPS3850-Q1 Other Parts Discussed in Thread: TPS3850 Hi Ti Expert
Does TPS3850 can support both Over voltage and Under Voltage monitoring?
as I found this statement in data sheet, but colleagues told me that it is not able to monitor both Over…
Part Number: TPS3850-Q1 Other Parts Discussed in Thread: TPS3850 Hi team,
Could you please confirm that if this IC can provide both over voltage and under voltage supervision for the single Sense input?
My understanding is that undervoltage and overvoltage…
Part Number: TPS3850-Q1 HI,
TPS3850-Q1 is not working properly, and the Reset pin is always low. The circuit diagram is shown below. Please help analyze the cause.
Thanks!
Part Number: TPS3850-Q1 Other Parts Discussed in Thread: TPS3850 Hi team,
Would like to check one question for TI TPS3850.
We would like to connect WDO of TPS3850 to NMI of SoC (DRA78x) as data sheet describes.
Due to we cannot disable NMI once it is…
Part Number: TPS3850-Q1 Other Parts Discussed in Thread: ADS7138-Q1 , TPS3435 While referring the Datasheet of the TPS3850-Q1 (watchdog) the VIL is 0.25V.
While referring Datasheet the VOL of the ADS7138-Q1 (ADC) GPIO pins is 0.2 x AVDD (since AVDD…
Part Number: TPS3850-Q1
The above shown image is operating characteristics of TPS3850-Q1:
Am a bit confused with the VIL and VIH from the datasheet. Its given as 0.25 and VIH is 0.8 the VOL of MCU is 0.45, so this will impact our design. Is these figures…