Part Number: TPS3852-Q1 Hi team
I would like to ask that does the TPS3852Q1 have the clamping input voltage protection? Is there any design recommendation for the set1 enable pin if customer want to use the ACC ignition point?
Part Number: TPS3852-Q1 In our application, WDI is 0.5Hz (1s tick - 1s on & 1s off), so to use TPS3852-Q1, the selected cap value is 33nF (based on below formula).
Need TI's confirmation to ensure this configuration (33nF) will work for 0.5Hz WDI.…
Part Number: TPS3852 Hi Teams,
Below is our currently WahctDog "TPS3851H33EDRBR" Circuit and Behavior:
- After ~56.68s no received the WDI single then Reset#/WDO# will go low to the EC25 module(RESET_N).
- Every 30s WDI send signal to reset watchdog…
Part Number: TPS3852 Assuming nMR has been pulled low to initiated nRESET to drop low for tRST.
Will the nRESET be 'cancelled' by pulling SET1 low during tRST?
Part Number: TPS3852 Hi,
We are seeing some strange behaviour around the TPS3852 in our circuit.
We are using feedback on the SET1 pin to enable and disable the watchdog. We have seen that disabling via SET1 during an active WDO event, terminated the…
Hi Ken,
You need a supervisor device, please make a post to the Power Management forum, you can use TPS3852 in the post to ensure your post will route to the power management forum correctly.
Part Number: TPS3852 Hi expert,
My customer wants to search for reset IC for their router application. CPU will assert a GPIO for reset and they want to cut off adapter power to system through a MOSFET under-controlled. After certain time period(2 seconds…
Part Number: TPS3852 Please give step by step procedure of TPS3852
We are trying but unable to get reset from TPS3852g33drbr
All the sequences are fine
Part Number: TPS3852 Hi,
This is Sanjay
I have developed a watchdog circuit using TPS3852G33DRBR on a General purpose Board and found not functioning. I have stopped the WDI pulse by making it continuous High or Low to get the RESET out. But, it is not…