Part Number: TPS3852-Q1 Tool/software: Hi,
I would like to know the values of input low current (IIL), input high current (IIH), output low current (IOL), and output high current (IOH) for TPS3852-Q1.
Thanks & regards
Priyanka S P
Part Number: TPS3852-Q1 Other Parts Discussed in Thread: TPS36-Q1 , TPS3436-Q1 We have a requirement as highlighted below -
Here, the requirement is clear as separate time based & window watchdogs.
Timing is not the issue here, but the type of watchdog…
Part Number: TPS3852-Q1 Hello,
I have the following schematics of the part:
The power supply is 3.3V and I am testing with a regulated power supply the voltage monitoring of the part. When I decrease from 3.3V to 2.5V the power supply, theoretically…
Part Number: TPS3852-Q1 Hi Team,
My customer find when they pull down the SET1 Pin to GND, the WDO/ still has the output, which is not matched with the following waveform.
Only when they re-start the device (power off then power on), the WDO/ can be shut…
Part Number: TPS3852-Q1
hi team,
could you help support this problem.
VDD to 3.3V, CWD to ground via 100pF capacitance, SET1=1 If the VDD voltage remains at 3.3V, What should the WDO output waveform state when the WDI input waveform is in the tPULSE …
Part Number: TPS3852-Q1 Other Parts Discussed in Thread: TPS3852 , Hello,
I received the TPS3852G33DRBR today and tested it on our circuit, but it didn’t work as expected.
The WDO works as expected if WDI stays high. I see the pulldowns every ~8…
Part Number: TPS3852-Q1 Other Parts Discussed in Thread: TPS3890-Q1 , TPS3852 , TPS3890 Hi Expert,
Our customer uses TPS3852-q1 in their project. But they don't use TPS3890-q1, which is suggested in datasheet as below. The SET1 pin is directly tied to 3…
Part Number: TPS3852-Q1 Other Parts Discussed in Thread: TPS3852 , TPS3703 , TPS3702 , LM4041-N , LM2903-N I have a question about the WDI minimum pulse duration spec.
Is it referring to 't' or 'd' in the picture below:
Part Number: TPS3852-Q1 Hi team
Need your help about 2 questions:
1. Please help to check the schematic whether it is ok: (could the reset pin be configured like this)
3852SCH.pdf
2. What are the normal operating current and quiescent current? What value…
Part Number: TPS3852-Q1 Hi team
I would like to ask that does the TPS3852Q1 have the clamping input voltage protection? Is there any design recommendation for the set1 enable pin if customer want to use the ACC ignition point?