Part Number: TPS386000 Other Parts Discussed in Thread: TPS62813M , TPS3704 Hi,
We are planning to use the following parts in our new design, I request to you please share the longevity information for the same.
1. TPS386000RGPT
2. TPS62813M
3…
Part Number: TPS386000 Hi,
I am using the part TPS386000RGPR. Can we short the CT pins and provide a single resistor to set the delay time?
Regards,
Nachiketh
Part Number: TPS386000 Hi,
I am using the part TPS386000RGPR.
1. Is it necessary choose the RSnL value as 10K ohms?
2. If its not what is the range in which we can choose the resistor value?
Regards,
Nachiketh
Part Number: TPS386000 Hello Team,
I have doubts with the watchdog timer function. The switch startup time will be long and I don't know if it will be able to send rising or falling edges early enough before the watchdog timer time out.
In the datasheet…
Part Number: TPS386000 Hi ,
We are using TPS386000 part. As per datasheet Watchdog timer (WDT) trigger input. Inputting either a positive or negative logic edge every 610 ms (typical) prevents WDT time out at the WDO or WDO pin.we are giving 5hz signal…
Part Number: TPS386000 Dear TI,
according to datasheet of TPS386000, the maximal current via output RESET pin is 5 mA.
Except of pull-up resistor at RESET line, I have a small capacitor (several nF) connected between RESET and ground. From measurement…
Part Number: TPS386000 Hi Team,
I am using TPS386000RGPR in my design. I would like to get the circuit design get reviewed by experts. TPS386000.pdf
I would also like to get a cofirmation regarding the unused pin status of WDO#, WDI and VREF. Whether…
Part Number: TPS386000-Q1 Hello,
I am looking for failure rate and mode information for part number "TPS386000QRGPRQ1". The information will help in FMEA activity.
Thanks
Part Number: TPS386000 Hi Team,
I am using TPS386000 in my design for voltage monitoring. Can we leave WDI# , WDO#, VREF and MR# pins floating if we dont want to use them in design.
Also can we connect all reset pins and consider single reset output…
Part Number: TPS386000 The component from the picture under was contained in the Reel with the label from the picture under.
Q1: Is the Reel relabeled?
Q2: Is this component marking valid? Is the quality of the component marking according to TI…