Part Number: TMS320F28075 Other Parts Discussed in Thread: TPS62441 , TPS65313-Q1 , TPS386000 Hi team.
TMS320F28075 Is there a power IC that meets the safety function? thanks
Part Number: TPS386000-Q1 Hello
Could you tell us the Absolute Maximum Voltage Ratings of VREF pin?
Datasheet described about current spec only.
Best regards
Yamane
Part Number: TPS386000-Q1 Hi team,
Even if adding an RC filter as a noise filter to 6 pin (SENSE 4 H), 7 pin (SENSE 4 L), will it be a problem as IC operation?
For accuracy such as error of voltage drop, the influence is considered.
I want to know if…
Part Number: TPS386000-Q1 Hello,
Customers are considering monitoring the battery supply voltage(12V) with TPS 386000-Q1. The customer Connect the power supply as shown in the attached figure.
12V is supplied to SENSE before 5V is supplied to VDD.
1)Can…
Part Number: TPS386000-Q1 Hi
I would like to know how this device operate when the SENSE voltage keeps at between Vhys+ and Vhys- as the following.
How the RESET signal will be if the SENSE voltage goes the above region in short time(Ta)? (Ta<Td)…
Other Parts Discussed in Thread: TPS386000-Q1 , TPS3700-Q1 Hello, The TPS386000-Q1 has the 1ch of Window Comparator input. Could you please let me know the use case of Window comparator of the TPS386000-Q1? I think that TI released Window comparator devices…
Part Number: TPS386000 The component from the picture under was contained in the Reel with the label from the picture under.
Q1: Is the Reel relabeled?
Q2: Is this component marking valid? Is the quality of the component marking according to TI norms…