Part Number: TPS38700 Hi,
My client needs a power-up timing control chip as follows:
1. Control 6 power supplies;
2. The maximum voltage is 5V;
3. The minimum power-on interval of each power rail can be controlled to about 200us;
4. It is best not to use…
Part Number: TPS38700 I had a question about the I2C address and the open drain/push-pull configuration.
How do we set the Pin driver configuration and I2C address when purchasing the part for evaluation. It would be helpful to know what the default…
Part Number: TPS38700 Hi Team,
My customer wanted to use EN[12:9] as GPO[12:9]. we cannot write in 0x20.
Regarding to the datasheet, "The alternate function can be enabled only if the corresponding PU/ PD/ SLP_EXIT/ SLP_ENTRY registers fields are all…
Part Number: TPS38700 Is there a linux driver available for the TPS38700? Or is there a part that is similar that I can use as the starting point of the of the TPS38700 driver?
Part Number: TPS38700 Hello,
I want to use the TPS38700 with as many sequencing outputs as possible, but the datasheet is very confusing.
There are mentions of all 12 being available in table 10.2, but table 10.1 immediately above says sequencer with…
Part Number: TPS38700Q1EVM Other Parts Discussed in Thread: TPS38700 Hi,
I am following the 4.3 Quick Start procedure in the User’s Guide: TPS38700Q1EVM Voltage Sequencer (snvu771a.pdf).
In the Device Scan Editor the TPS38700x is listed
However…
Part Number: TPS38700-Q1 Hi Expert:
Our customer has start design TPS38700-Q1 Sequencer for Nvidia ADAS automotive application. but datasheet doesn't include Package information with the complete PN.
could you please help provide package and order…
Part Number: TPS38700 Hello,
A few questions regarding the TPS38700:
I would like to evaluate the TPS38700 GUI, but the link leads to the FUSION POWER DESIGNER which doesn't have the TPS38700 in the list of available devices. How can I access the…
Part Number: TPS38700-Q1 Other Parts Discussed in Thread: TPS38700 Hi team,
Due to EOL of Intel power device: ES1030QI , c ould you please help suggest whether TPS38700 is suitable as the alternative device? Please correct me if you have better suggestions…