Part Number: TPS3852-Q1 Other Parts Discussed in Thread: TPS3890-Q1 , TPS3852 , TPS3890 Hi Expert,
Our customer uses TPS3852-q1 in their project. But they don't use TPS3890-q1, which is suggested in datasheet as below. The SET1 pin is directly tied to 3…
Part Number: TLV840-Q1 Other Parts Discussed in Thread: TPS3890 , TPS3808 Dear TI team,
I am looking for reset IC which can implement 10s~1min reset time. If reset voltage level can be adjustable, that will be perfect.
Could you suggest solution with me…
Part Number: TPS3850 Other Parts Discussed in Thread: TPS3430 , TPS3890 , TPS3851-Q1 , Hello experts
Are there any supervisor devices similar to the TPS3850 that can support a 5 second reset delay?
Thanks,
Jim B
Hi Antonio,
You could always use the TPS3890-Q1. This device has fixed threshold options, an adjustable version, and a sense pin. The TPS389033-Q1 is made for a 3.3V input.
Thanks, Abhinav.
Part Number: TPS3809 Other Parts Discussed in Thread: TPS3840-Q1 , TPS3890-Q1 Hi Sir
Why we can't find TPS3809J25QDBVRQ1 in web order info? is this part still available?
If there is not available, may you can suggest P2P replace part?
…
Part Number: TPS3809 Other Parts Discussed in Thread: TPS3890 , TLV803 , TPS3808-Q1 , TPS3808 , TPS3838-Q1 , TPS3890-Q1 Hi Sir
Because customer need automotive rating device,
May we use TPS3809K33 to replace UM803RS? what thing we need to notice?
May we u…
Hi Ross,
I looked over the schematic and I believe the LDO output will be roughly the ADJ voltage (1.23V) when SENSE is low because /RESET is pulled "low" due to undervoltage condition at SENSE which would then put R222 in parallel with R221 which would…
Part Number: TPS3840 Other Parts Discussed in Thread: TPS3890 Hi,team
I am looking for an IC to monitor a 24V power supply.
I have two questions.
Q1.
I'm considering TPS3840, but I'd like to ask a question about Equation (8) in the datasheet…
Aaron,
1. TPS3808G01 is adjustable with external resistors. This device can monitor 1.425V or any voltage above the VIT threshold for this device which is 0.405V. The TPS3808G01 has +/- 2% accuracy that follows normal Gaussian distribution and the main…