Part Number: TPS3895 Hi all,
I have a question about TPS3895.
On the horizontal axis of the graph, Which is the temperature, Tj or Ta ?
The graph is shown on p.1 or p.9(Fig.8) of the data sheet.
I think it is Ta because the following is described…
Part Number: TPS3895 Hi Team,
Would it be OK if I connect Vsense directly to the SENSE pin without a resistor divider?
It seems that a resistor divider is needed to meet the requirement highlighted below, but I don't quite understand why this requirement…
Part Number: TPS3895 How do I calcuate "SENSE Threshold Overdrive Voltage percent" to determine the "SENSE Pulse duration" in Figure 9 of the datahsheet? In my application, I have addition hysteresis resistor Rh.
Part Number: TPS3895 Hello TI Team,
We are currently working with the TPS3895A and would like some confirmation on my understanding of the sense pin immunity and output delay.
The falling output delay is specified as 16us. It is my understanding that…
Part Number: TPS3895 TPS389x's Isense_out is described on datasheet page-5, please let me confirm about two points below;
①What is the mean of Min: 0.0003A?
For example, are Minimum spec mean device variation or specified condition?
If device…
Part Number: TPS3895 Hi
I use the TPS3895ADRYR as a power on reset signal.
The target voltage= (1+511k/110k)x 0.5= 2.82V.
I know TPS3895A output is push-pull , so I depopulate the R746.
However, I can't see the reset (output) release to high level…
Part Number: TPS3895 Hi expert,
My customer is using TPS3895 to protect F28377s's 1.2V core voltage with below circuit design. They tested with suddenly cut off the 1.2V power supply when MCU is running, but the power stage is damaged. Do you have any…