Part Number: TPS3899 Other Parts Discussed in Thread: TPS3851 dears,
My customer is seeking for 20s and 50s delay watch dog, i'd like to recommend TPS3899 for lowest cost, but according to the datasheet, the max delay time is 6.2S with 10uF capacitor…
Part Number: TPS3899-Q1 Hi Team,
In our circuit design featuring the Voltage Supervisor ( TPS3899DL31DSERQ1 ), we've set the undervoltage threshold to 3.1V. However, during RF data transmission, the voltage drops below this threshold, triggering the interrupt…
Part Number: TPS3899 Actually we are planning to used this part in our one of the design but the issue is this actual part having the pitch different as compared to the pcb footprint recommendation due to which the components leads not sit properly on…
Part Number: TPS3899 Hi,
we are planning to use the following parts which are mentation in the datasheet. but actually not available on TI website, mouser and Digiky.
will it be available on demand or in the future.
TPS3899DL12DSE,TPS3899DL16DSE, TPS…
Part Number: TPS3899 For detect time delay (td-sense), for example, when CCTS_EXT: 1μF is used, there is a slight difference between the value on page 5 of the data sheet and the calculation formula on page 14.
・Page 5: 619ms
・Page 14: 655ms
Am I…
Part Number: TPS3899-Q1 Other Parts Discussed in Thread: TPS3899 Hi,
In the datasheet of TPS3899-Q1, I don't understand Figure 7-3:
1. What is the meaning of "VDD=SENSE", is the two pins connect together?
2. Since the width of positive pulse…
Part Number: TPS3899-Q1 Other Parts Discussed in Thread: TPS3899 Hello,
Earlier we are using LTC2954CTS8-1#TRMPBF, Now we are planning to replace with TPS3899DL01DSERQ1.
Could you please review the connection of power ON/OFF control IC TPS3899DL01DSERQ1…
Part Number: TPS3899 Hi,
I want to confirm the behavior on TPS3899.
If the pulse (Low->High->Low) whose width is less than tD (Red circle) enters on SENSE pin, TPS3899 /RESET is Low to High (Yellow arrow), after High to Low on this SENSE pin. Is…