Part Number: TPS3899 Hi,
On TPS3899-DL (Open Drain) device, could you please let us know the rise time on /RESET pin with typical pull-up (10k-ohm?) ?
Also, could you please take the waveform during rising on /RESET pin on EVM?
My customer requests…
Part Number: TPS3899 Hi Team,
Our customer is looking for a PSpice model of TPS3899 that would work with Cadence Allegro 2019. Do we have an old PSpice model of TPS3899? Please see the details of his inquiry below.
Your TPS3899 spice model is very…
Part Number: TPS3899-Q1 Are there minimum and maximum values for the Negative-going input threshold for adjustable sense threshold TPS3899DL01DSERQ1?
The datasheet only specifies a typical value, which does not support calculation of upper and lower…
Part Number: TPS3899 Hi,
On the datasheet of TPS3899DL26DSER, VIT = 2.548V~2.652V (2.6V±2%) and VHYS = 0.078V-0.182V (2.6V * 3% - 2.6V * 7%) under all temperature range, Which is HYS voltage (VIT + VHYS)? "2.6V + (0.078V-0.182V)" or "(2.548V~2.652V…
Part Number: TPS3899-Q1 Other Parts Discussed in Thread: TPS3899 Hi,
In the datasheet of TPS3899-Q1, I don't understand Figure 7-3:
1. What is the meaning of "VDD=SENSE", is the two pins connect together?
2. Since the width of positive pulse on…
Part Number: TPS3899 Hello,
1. I tested the TPS3899 PSpice Transient Model (Rev. A) and the TPS3899DL_PSPICE_TRANS.DSN error opening the file on OrCAD 17.4 pspice
2. The TPS3899DL_PSPICE_TRANS.lib is not working on LTspice - error in file
Note…
Part Number: TPS3899 Other Parts Discussed in Thread: TINA-TI , PSPICE-FOR-TI Hi Team,
Our customer downloaded the TPS3899 model on the product page but was unable to import these model into his system.
I have instructed the customer to follow this…