Part Number: TPS3899-Q1 Other Parts Discussed in Thread: TPS3422 , TPS3899 Tool/software: Hello, We are considering TPS3899-Q1 for our design. Our use case conditions are as follows: 1. If the push-button connected to sense pin is pressed for a duration…
Part Number: TPS3899-Q1 Hi Team,
In our circuit design featuring the Voltage Supervisor ( TPS3899DL31DSERQ1 ), we've set the undervoltage threshold to 3.1V. However, during RF data transmission, the voltage drops below this threshold, triggering the interrupt…
Part Number: TPS3899-Q1 Other Parts Discussed in Thread: TPS3899 Hi,
In the datasheet of TPS3899-Q1, I don't understand Figure 7-3:
1. What is the meaning of "VDD=SENSE", is the two pins connect together?
2. Since the width of positive pulse…
Part Number: TPS3899-Q1 Other Parts Discussed in Thread: TPS3899 Hello,
Earlier we are using LTC2954CTS8-1#TRMPBF, Now we are planning to replace with TPS3899DL01DSERQ1.
Could you please review the connection of power ON/OFF control IC TPS3899DL01DSERQ1…
Part Number: TPS3899-Q1 Are there minimum and maximum values for the Negative-going input threshold for adjustable sense threshold TPS3899DL01DSERQ1?
The datasheet only specifies a typical value, which does not support calculation of upper and lower bounds…
Part Number: TPS3899-Q1 Hello,
My customer considers using the TPS3899DL01DSERQ1 with the follwoing conditions.
How does RESET# work when V1 power is shorted to GND or V1 power is not supplied due to a disconnection?
Thank you.
JH
Hi Vitaliy,
The TPS3899 has a programmable sense delay which will require the SENSE pin to stay below threshold longer than tsense programmed before RESET goes low. For this device the maximum programmable time is 6.5s.
https://www.ti.com/product/TPS…
The p2p device will be TPS3808G18QDBVRQ1.
I would highly recommend you to look at newer product like TPS3899-Q1 which has improved performance in terms of Iq, size.
https://www.ti.com/product/TPS3899-Q1
More voltage options in commercial grade also av…
Part Number: TPS3840-Q1 Other Parts Discussed in Thread: TPS3899 Hi Team,
Do we have more appropriate solution that can replace XD6132C10E? P2P is better, thank you.
Regards,
Roy