Part Number: TPS40055
Hello,
I've spent the last five months designing and creating the attached SwitcherPro Design schematic using the TPS40055. After many weeks of debugging, I've found that your generated design has some faults. I'm hoping someone…
Part Number: TPS40055 Other Parts Discussed in Thread: LM5145 Hi
Below is the sw waveform.
If bandwidth is 20MHz, max voltage is 36.5V. If bandwidth is FULL, max voltage is 59V. Let me know if I can use it.(Max voltage of SW = 45V) Below is a zoom…
Part Number: TPS40055 Hi
It acts as if it had been latched intermittently.
1. Does the latch work if excessive noise is applied to the KFF(#1) pin?
2. Is there a condition that another pin can be a latch?
Thanks
Part Number: TPS40055 Other Parts Discussed in Thread: LM25145 Hello Guys,
Good day.
Our customer is looking for the ESD rating both HBM and CDM for TPS40055PWP.
Appreciate your help on this.
Thanks in advance!
Art
Part Number: TPS40055 Hello team,
My customer is trying to replace external FET due to EOL.
By changing external FET, is compensation network change usually needed?
Updated FET will have much smaller parasitic capacitance. Rise and fall time will…
Part Number: TPS40055 Buck regulator team,
Can you tell me what the "G4" suffix means for TPS40055? In the datasheet, it's not clear what the difference is between:
TPS40055PWPR
TPS40055PWPRG4
Thanks,
Darren
Part Number: TPS40055 Hello TI Experts,
My customer wants to design with TPS40055, and they want to enable/disable IC using SS/SD pin.
please check the schemes below, which is right or not.
schematic 1 ;
schematic 2 ;
the difference is only…
Part Number: TPS40055
Hello
I designed DC/DC Converter using TPS40055
But Sometimes Not Start up when Power on.
Condition:
VIN : 20V
VOUT : 12V
CH1 : SW
CH2 : IOUT
CH4 : VOUT
Connect the 2A LOAD
No Load
what reason…
Part Number: TPS40055 Other Parts Discussed in Thread: TPS40051 Hello guys,
One of our customers is using TPS40051 now for their current products and they are considering replacing the device with TPS40055 because TPS40055 current limitter accuracy…