Part Number: TPS40060 Other Parts Discussed in Thread: LM5145
Tool/software:
According to TI website, TPS40060 max. output current is 10A. TPS40060 data sheet, product information and support | TI.com What are factors that put this limitation and what…
Part Number: TPS40060 Other Parts Discussed in Thread: LM5146 , LM5145 Hello Team,
My customer is requesting the thermal information for the device TPS40060PWP. Can you share the information with us?
Regards,
Renan
Part Number: TPS40060
Hi, team:
When my customer test TPS40060 found out the the output signal abnormal:
The green: PMOS ; The blue: NMOS
It look like mos go-through due to too long Ton.
I couldn’t find description about dead time in datasheet…
Part Number: TPS40060 Other Parts Discussed in Thread: LM25145 , LM5145 Hello,
I'm using a TPS40060 device. This IC drives a Pch FET as a high-side FET. However, recently, Pch FET is not readily available. So I want to use high side FET with Nch in this…
Part Number: TPS40060 Dear,
our client power spec was need 85W, and input normal 24v, Output voltage/current:20V/4.25A
TPS40060 can meet spec?
if any suggestion, Please advise me.
Thanks,
Best regards,
Lawrence.
Part Number: TPS40060 Hello Concerned Person,
I am using TPS40060 in my design. The design has following specs.
Vin_min= 36 V
Vin_max= 50 V
Vout= 5 V
Iout=5
Fsw=250 KHz
While reading data sheet of product I could not understand that which is the pin…
Part Number: TPS40060 Other Parts Discussed in Thread: TINA-TI , LMR36015 Tool/software: WEBENCH® Design Tools Dear
Can you check my circuit for me? Why the fever is so serious,
using environment: DC48V INPUT, DC12V/1A OUTPUT,
TINA-TI tools are not familiar…
Part Number: TPS40060 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models
I am attempting to simulate the circuit above.
U1's symbol definition is defining duplicates for "t"
I am using the " TPS40060…
Part Number: TPS40060EVM Other Parts Discussed in Thread: TPS40060 , , LM5146 , LM5145 I want to use the TPS40060EVM board to characterize the TPS40060 buck IC by some measurements. I also intend to do some simulations as well. Is it possible to get the…
Hello Community,
Is it possible to convert a voltage with the Value 30V to 42V to a voltage with the value 20V ? I'm not sure, because in the maximum ratings is indicated the following: Output voltage range COMP, RT, KFF, SS: –0.3 V to 6 V.…