Other Parts Discussed in Thread: TPS40120 , UCC39002 , TPS40210 One of project needs high o/p current. So I connected three TPS40120 in parallel. As shown below: (below shown is 2 parallel DC-Dc, similarly I connected three in parallel)
But when I…
Other Parts Discussed in Thread: TPS40210 , INA213 , TPS40120 Hi
I'm using the TPS40210 as a boost converter. Actually, I'm working on an unmodified 40120EVM board atm.
I need to dynamically adjust the output slightly and my plan was to inject a…
Other Parts Discussed in Thread: TPS40210 Hi,
Form previous help in this forum, I had successfully generated +100V output from +12V by using TPS40210 in a TINA simulation. ( TPS40210 cannot boost up to 100V output )
My next step is to generate both…
Part Number: TPS40210 Other Parts Discussed in Thread: TPS40120 , Dears,
Customer use TPS40120 in the Sprinkler head drive,when they do the function test,then found the load capacity is insufficient,details pls kindly find below information:
1.DC…
Hello,
The UCC3806 is a dual output controller though it can be used in a flyback where only one of the outputs are used to drive the switch it might be better to choose a single output controller. Look at page 46 of the attached under General Purpose…
Siyu,
I think the toggle flip-flop in the block diagram on page one of the spec should have let you know that the max you will get with this device is 50% duty.
Go to page 43 and 44 of the attached and select a more suitable part.
Peter,
i am enclosing the Power Management Guide for 2011. The section you will be interested in starts on page 43 and actual devices listed on page 46, With the minimum information you have given me I would expect that you will want something like…
Part Number: TPS40210 Other Parts Discussed in Thread: LM5155 I am doing a design with TPS40210 with 15V IN(min) , 19.2V INNOM) , 22.8V IN(MAX) with V OUT = 24V I OUT = 3A. When I start a PMIC design I usually bring the equations into a CAS (Computer…