Part Number: TPS40170-EP Team,
Could you suggest us a buck converter which meets MIL-STD 1275 & MIL-STD 461.
Required specification are as below,
Input voltage: 28V typical
Output voltage : 5V or 12V
Output Current: 6A to 8A
Switching frequency between…
Part Number: TPS40170-EP Other Parts Discussed in Thread: TPS40170 Cluster_Cranking_Sheet updated.pdf
HI Team,
We have designed an circuit for crank simulation with referecnce of TI TPS40170.
Kindly check the circuit and let us know if any mistakes in…
Part Number: TPS40170-EP Other Parts Discussed in Thread: TPS40170 , LM5145 Cluster_Cranking_Sheet-1.pdf We have modified the circuit as TI team guided us. kinldy check the modified circuit and provide your feeback. FYR please check the previous post for…
Part Number: TPS40170-EP Dear Team,
I am facing license call error message in my PSpice software, I unable to simulate my schematics.
Error message ID : LMC-18952
Kindly suggested solution for this license issue.
Part Number: TPS40170-EP Other Parts Discussed in Thread: TPS40170 , LM5145 We designed a circuit to simulate the car self motor cranking. We need to verify our circuit design to proceed PCB manufacturing. Please suggest us if any mistakes in circuit or…
Hi Ilan,
1. First thing that I would try is to test the TPs40170-ep design on the bench using resistive or electronic load to make sure - if you see any issues. Does the design operate over the full load range that you expect to operate in your system…
Part Number: TPS40170-EP Other Parts Discussed in Thread: TPS40170 Tool/software: Webench Hi,
i have to design DC2DC 28v to 7.4v with peak current 5A Ton=0.5msec base on TPS40170.
the stady state is 0.5A .
what is the considration to take in the design…
Other Parts Discussed in Thread: TPS40170-EP , TPS40170 We're using the TPS40170-EP in a 12V->5V application.
I've added an overvoltage protection crowbar to the output, which short circuits the regulator output if an over-voltage condition is detected…
Other Parts Discussed in Thread: TPS40170 Hi - Our company uses Altium 13 for our schematic capture and PCB layout. The part TPS40170 has a PSPICE model on its website but it is only for Cadence. Could I either get an encrypted version that works with…