Part Number: TPS40170 Other Parts Discussed in Thread: LM5143-Q1 Hi team,
my customer noticed that the TPS40170 has frequency synchronization master/slave option. Do you know if they can put two TPS40170 in parallel to achieve supply redundancy?
Thank…
Part Number: TPS40170-Q1 Other Parts Discussed in Thread: LM5141 , LM61460 , TPS40170 Hi,
I have a question about DC DC Converter. The question is that, in light load, the converter quescient current is 25mA. But I want to decrease this current in no load…
Hi,
For interleaved operation mode connection, you can refer to 9.2.2 section of the datasheet. For LM5143-Q1 FB and COMP connection, I guess you can use same architecture of the close-loop control but due to different control between TPS40170 and LM5143…
Part Number: TPS40170 Dear TI members
I am reviewing the schematic of my co-worker but have some question related to TPS40170
Q1) Input voltage : 12~24[V] , output voltage : 12[V]
I think that there is a problem when the input voltage is apply to 12…
Part Number: TPS40170 Other Parts Discussed in Thread: LM25119 , LM5143-Q1 , LM5140-Q1 Hi TI,
Kindly suggest me the best suitable dc-dc converter.
Requirement
Input: 12V
Output: 11V/ 50Amax
I couldn't find suitable converter.
So, Can I use TPS40170…
Part Number: TPS40170 Other Parts Discussed in Thread: LM5146-Q1 Hello everybody,
Our product using TPS40170 failed on EMC radiated test at ~96MHz - so it's definitely common-mode noise problem! We narrowed it down with EMC probes and Spectrum Analyzer…
Part Number: TPS40170 Dear Specialists,
My customer is confirming TPS40170 and has a request.
Could you please advise?
---request
I am confirming SLVA582A(TPS40170-Q1 Pin Open and Short Test Results)
I'd like to see actual data, can you arrange it?…
Part Number: LM5022 Other Parts Discussed in Thread: LM5117 , LM5145 , LM5116 , TPS40170 , LM5020 , UCC28C40-Q1 Tool/software: WEBENCH® Design Tools The table on the website says 1.25V for Vout min, but Webench rejects anything under 6V.
I am interested in…
Part Number: LM5170-Q1 Other Parts Discussed in Thread: LM5170 , LM25117 , TPS40170-Q1 Hello all,
I wish to use LM5170-Q1 (Multi phase controller ) , in my system design . The aim is to create switch mode power supply . As this IC can be digitally controlled…