Part Number: TPS40200-HT Dear Sir,
Can you recommend or know if there is an updated / or similar synchronous version of TPS40200-HT (this part number is non-synchronous). We at 153'C ambient. 43V input and 24V output at 1.37A. Downhole environment.…
Part Number: TPS40200-HT I want to design an isolated buck converter with an input voltage range of 16 VDC to 48 VDC and an output of 5 V at 3 A. I have selected the TPS40200-HT for high-temperature operation. Could you please assist me in developing…
Part Number: TPS40200 Tool/software: Hi TIer
My customer would like to use the TPS40200 as an RC resonator and thus as a transmitter for wireless charging. Customers have discovered this application from other customer products. Do we have corresponding…
Part Number: TPS40200 Other Parts Discussed in Thread: LM25149 Hello,
I’m currently evaluating a TPS40200 for use in a DC-DC buck converter application and would appreciate some clarification.
My design involves stepping down from 36V to 12V, with…
Part Number: TPS40200 Please help me choose a DC-DC converter without thermal shutdown.
Here are the main specifications:
MAX input voltage - 15- 33 V
Output voltage - 13 V
MAX output current - 0.5 A.
I found the TPS40200 chip, which might work…
Part Number: TPS40200 Hello friends. I need to design a converter with two outputs +13 and -13 volts 0.3 A. With the possibility of current limiting. Input voltage 15-32 volts. It is also important that the microcircuit does not have internal thermal…
Part Number: TPS40200 Tool/software: Using the TPS40200 in a 50V input, +5V configuration. Initially was tripping the common mode aspect of I sense pin. Connected small ceramic from pin 5 to 8 and that was solved. Now have an improved layout with this…
Part Number: TPS40200 Problems applying TPS40200 part. Designed a 50 to 5V at 500ma buck with this part. It seems to go into overcurrent hiccup mode at anything over 200ms output. I shorted the sense resistor and nothing changes. I extended the soft start…
Part Number: TPS40200 I need an unencrypted SPICE model for the TPS40200 that is correct and that I can pull into LTSpice. Although there is " TPS40200 Unencrypted PSpice Average Model Package (Rev. E) - SL VJ006E.ZIP - ", it doesn't appear to have the…