Part Number: TPS40200 Tool/software: Hello Ti,
I was looking at the overcurrent voltage threshold tolerance (ViLim) for the TPS40200 and the datasheets states that it is from 65mV to 140mV, typically 100mV from the 0'c<Ta<125'c range. This is a bit…
Part Number: TPS40200-EP Other Parts Discussed in Thread: TPS40200 Tool/software: What is the difference between TPS40200MD and TPS40200MDREP?
Are they the same product?
What does REP mean?
EP seems to mean Enhanced Product, does it mean equivalent or…
Part Number: TPS40200-HT Tool/software: Hi, good day,
I would like to design a high temp buck converter with TPS40200-HT but it is near impossible to find a P-MOS that works up to 200ºC. Would be possible to use a SiC N-MOS like G3R450MT17D 1700V 450mΩ…
Part Number: TPS40200 Tool/software: The link to the white paper appears to be broken
I have visited the web page for archived PSDS resources, but for this particular one the link doesn't work.
Please send me the pdf.
Thanks,
Bob Sachsalber
…
Part Number: TPS40200 Hi ,
During a static electricity test, a phenomenon has occurred where the output decreases when static electricity is applied. After the output drops, it will immediately return to normal output voltage.
The phenomenon starts…
Part Number: TPS40200-HT Other Parts Discussed in Thread: TPS40200 Hello,
I have used successfully TPS40200-HT for input voltages higher than 15V.
I have problems with the TPS40200-HT for input voltages lower than 15V. I want to use a 6V input for…
Part Number: TPS40200 Hi Team,
Our customer has an existing design with TPS40200 and they intend to upgrade to its high temperature version TPS40200-HT. They reviewed the datasheets to see if there are any adjustments needed but it seems that there…
Part Number: TPS40200 I have a question about the switching loss over the Buck converter diode on page 22 of the datasheet of TPS40200
https://www.ti.com/lit/gpn/tps40200
My understanding is that the diode junction capacitance (also diffusion capacitance…