Part Number: TPS40200-HT Dear Sir,
Can you recommend or know if there is an updated / or similar synchronous version of TPS40200-HT (this part number is non-synchronous). We at 153'C ambient. 43V input and 24V output at 1.37A. Downhole environment.…
Part Number: TPS40200-HT I want to design an isolated buck converter with an input voltage range of 16 VDC to 48 VDC and an output of 5 V at 3 A. I have selected the TPS40200-HT for high-temperature operation. Could you please assist me in developing…
Part Number: TPS40200-HT Tool/software: Hi,
The footprint of TPS40200HKQ on the Ultra librarian is a normal IC footprint with Pin1 starting at left. According to the first page of the datasheet, Pin1 is top right corner. Is that correct?
The ultra…
Part Number: TPS40200-HT Tool/software: Hi, good day,
I would like to design a high temp buck converter with TPS40200-HT but it is near impossible to find a P-MOS that works up to 200ºC. Would be possible to use a SiC N-MOS like G3R450MT17D 1700V 450mΩ…
Part Number: TPS40200-HT Other Parts Discussed in Thread: TPS40200 Hello,
I have used successfully TPS40200-HT for input voltages higher than 15V.
I have problems with the TPS40200-HT for input voltages lower than 15V. I want to use a 6V input for…
Part Number: TPS40200-HT Hi,
I have Power supply that use your 2 of TPS40200SHKJ for +13V and -13V. we have an issue with idle current (No load status) which drain from 20mA to 40mA in high Temp (150 -175C) and we didn't have this problem before,…
I've chosen the bigger MOSFET package thinking that it will help with heat dissipation - system rated 175C. On the actual board, the MOSFET temperature is 87F, Inductor 85F, TPS40200-HT 89F in a 77F room temperature - maybe this is not so bad. What worried…