Part Number: TPS40200-Q1
Hi team
Could you please tell us V ILM on V DD : 9.0~16.0V and T A : -30~+85℃? If V ILM is in 80mV~120mV on this situation, it is acceptable.
Regards,
Iza
Part Number: TPS40200-Q1 This chip can meet the requirements of input 5V, output 4V/2.5A buck, 100% duty cycle, 1mA light load efficiency of about 90%?
Is there a more suitable recommendation?
Part Number: TPS40200-Q1 Other Parts Discussed in Thread: TPS40200 Hi Team,
Can you verify what the operating Junction temperature is for the TPS40200-Q1? Looks like the datasheet only specifies this as an ambient temperature:
Thanks!
David
Part Number: TPS40200-Q1 Other Parts Discussed in Thread: TPS40200 , LM5116 Hello TI,
I want to use the TPS40200 for my design it is however a "P-channel FET Driver", I want to drive a N Channel FET. I was thinking inverting the GDRV signal to drive…
Other Parts Discussed in Thread: TPS40200 I need to sync clock between two TPS40200 to avoid sub harmonic, one VOUT is 3V3 (Master, source clock from RC circuit) and one VOUT is 1V8 (slave). Typical current is 50mA and 200mA respectively.
How this is…
Other Parts Discussed in Thread: TPS40200-Q1 I recently purchased the TPS40200-Q1 and I am attempting to design a DC/DC converter based on the SwitcherPro Design with the following specifications:
Vin(min) = 7.4V
Vin(max) = 12.4V
Vout = 6.25V…
Hello Reza,
I tend to agree with Kai that with good component placement and wide traces for high current GND paths back to Q1 GND, that a single ground plane can work best. I think Kai meant to say don't connect pins 4,5 of U2 to the ground plane though…
Other Parts Discussed in Thread: TPS40210-Q1 , TPS40200-Q1 Dear, All
As for the datasheet of TPS40210-Q1, the operating temperature range is indicated by Tj. However, to the datasheet of buck type TPS40200-Q1, the operating temperature range is indicated…
Hi Mitchell,
So we typically don't have a negative input to negative output buck converter, and don't recommend you do that with the LMR38025. What you can do is use a PWM controller to do so, as shown here: /cfs-file/__key/communityserver-discussions…
Hi Shinichi,
Sorry for the long delay and thanks for already looking at other e2e threads to find an answer.
1. LM5001 is an asynchronous boost converter. It should work for this application, but there are also newer converters with similar specs…