Other Parts Discussed in Thread: TPS40210 Hello,
I have asked about PowerPAD and E2E answer was it is connected to GND terminal internally.
http://e2e.ti.com/support/applications/automotive/f/26/t/383156
Please answer following question about…
I would like to confim the value of VGDRV.
I have questions.
1. How much is the value is VGDRV with VDD=12V? I think it is 4V, but there is not the specification of VGDRV.
2. Does VGDRV change by VDD value? In the case of VDD = 6V, how much is VGDRV…
Part Number: TPS40210-EP Other Parts Discussed in Thread: TPS40210-Q1 , TPS40210 I find in the product filter page the output voltage range of TPS40210-EP is (7-9)V. My application need a 105V output.
I make a design at Webench power design and find…
Hi Joshua,
Thanks for using the e2e forum. All features and functioning are described in the datasheet of the TPS40210 device. There is additional information on quality, reliability and packaging on the according product page of the device. Please…
Other Parts Discussed in Thread: TPS40210-Q1 , TPS40210 Hello,
I believe that the datasheet for the TPS40210-Q1 Boost controller contains an error in the formula for calculating the critical output current. The datasheet defines the critical current…
Hi Egidijus,
Thanks for using the e2e forum. From functional side, there should be no differences between catalog and automotive version. They have the same features and should behave identical within the recommended operation conditions. However, the…
Hi, Mr. Reddy:
Thank you for your inquire. Yes, UCC28730-Q1 can support 12V/1.5A by some design changing such as transformer, Rsense..etc. However, to enable UCC28730-Q1, it is needed to provide 21V to UCC28730's VCC. Thus, UCC28730-Q1 can not operate…
I think I know what the issue is. I'm using the TPS40211-Q1. The design guide I followed is for the TPS40210-Q1.
The TPS40211-Q1 ref voltage is 260mV. The TPS40210-Q1 ref voltage is 700mV.
I will correct for this and report back with results.
Part Number: LM5022-Q1 Other Parts Discussed in Thread: TPS40210 , LM5022 , TPS40210-Q1 , Hello TI,
I have question about TPS40210 & LM5022 output vpltage capbility.
Why LM5022 just can operation output voltage up to 300V? and why output voltage minmum…
Other Parts Discussed in Thread: TPS40210-Q1 Hello, My customer has some guestions about TPS40210-Q1 datasheet. (SLUS772F)
[Q1] Does VOCP described in the section "8.2.2.6 Current Sense and Current Limit" mean VISNS?
[Q2] This question is same [Q1…