Other Parts Discussed in Thread: LM5022-Q1 , LM5121-Q1 , TPS40210-Q1 , LM5121 Hi Team,
One of our customer is designing boost converter for below spec for automotive application and we suggested LM5121-Q1, LM5022-Q1 and TPS40210-Q1 for the application…
Hi Kai,
We are currently looking into this issue with the LM5121. We will get back to you shortly.
You can try the inputs (46V to 50V Vin, 52V Vout, 4.8A Iout) in WEBENCH and I get the following products (LM5022, LM5022-Q1, TPS40210, TPS40210-Q1)…
Thank you for considering the TPS40210-Q1 in your project. If the design is generated by Webench, it should work. I am afraid there is a mistake somewhere when copied the Webench design to layout your PCB, or a wrong part is used. Please capture a few…
Hello Ranjanir-san,
Thank you for your reply.
SEPIC simulation is request form TPS40210-Q1 customer, so p lease answer my question when correct person return to work.
Best Regards.
Part Number: TIDA-00281 Other Parts Discussed in Thread: TPS40210-Q1 , UCC27201A In the TI Design TIDA-00281, in the flyback circuit, they have used a isolated flyback transformer 750315511 mfg. @Wurth Electronics. But i was unable to find that in any…
Other Parts Discussed in Thread: TPS92690 , LM3478 , LM3488 , LM3481 , TPS40210 , TPS40210-Q1 , LM5022 , LM5022-Q1 Hi I am satya.I am new to the forum. I am working on a project led drivers
After going through different ICs i zeroed on TI webench tool…
I have entered that datas (input=6-12V and Output =12V/3A) and
following components are suggested and designing works. LM5122, LM5122-Q1, TPS40210, TPS40210-Q1
Here is the result for different inputs.
2248.LM5122.pdf
Hi Hirano-san,
Q1/Q2: There is no maximum current limit setting for the device. TPS40210 uses external power stage components (Inductor, MOSFET, diode). These components and the layout must be robust enough to support the peak current requirements.…
Other Parts Discussed in Thread: TPS40210 , UCC28C43 , UCC28C55-Q1 Hello Team,
I want to design the power supply with below specification.
Input : 48V
Output : 3500Vdc, 3mA
Protection : Overvoltage, Overcurrent, short-circuit.
Isolation : Yes…