Part Number: TPS40210-Q1 Other Parts Discussed in Thread: TPS40210 , TPS40211 Hello,
is it possible to use the TPS40211 as an alternative for the TPS40210 by just adapting the feedback network, or do we have to expect any other regulation behavior because…
Part Number: TPS40211 Hello,
I would like to know The calculation method of Cout and ESR is not found in the data sheet. How is the number in the red box calculated?thanks.
Part Number: TPS40210 Other Parts Discussed in Thread: TPS40211 , TL431 I would like to be able to use a circuit similar to PMP6963 with both the TPS40210 and TPS40211 devices. I understand there will need to be changes to the feedback\compensation passive…
Part Number: TPS40211 Other Parts Discussed in Thread: TPS40210 , LM5155 , LM5176 HI,
I want to design a programmable PSU with input range of 4.5V to 22V and a variable output 0 to 5V with current of about 2~4A[ maximum total power 20W ].
the Vout voltage…
Part Number: TPS40211 Hi, Customers want the soft start time to be as long as possible. However, there is no information about the maximum value in the data sheet. Could you tell me the recommended maximum value of the soft-start capacitor? And Please tell…
Part Number: TPS40211 Hello,
I want to use TPS40211 to make a LED driver.
I found the way to set LED current at P35 of datasheet.
How can I set the Max output voltage?
Input voltage: DC12V-24V
Output: Max 48V at 1A
Thank you!
I think I know what the issue is. I'm using the TPS40211-Q1. The design guide I followed is for the TPS40210-Q1.
The TPS40211-Q1 ref voltage is 260mV. The TPS40210-Q1 ref voltage is 700mV.
I will correct for this and report back with results.