Part Number: TPS40305 I am adapting an existing TPS40305 design to use the controller to supply a current to a load. The load needs a 5A current driven through it during state one but it needs up to 20A driven through it during state 2. The requirement…
Part Number: TPS40305 Hi
Base on Datasheet EN/SS pin need to be Floating in order to turn on, but how can I connect this to the microcontroller so I can control it.
Thank you
Part Number: TPS40305 Other Parts Discussed in Thread: TPS40428 Tool/software: WEBENCH® Design Tools Hi, Mr/Miss ,
I have got a really puzzled problem about TPS40305 controlling ...
in my power system , TPS40428(gen 0.85) --> TPS40305(1.8V) --> TPS40305…
Part Number: TPS40305 Other Parts Discussed in Thread: TPS40304 Hi,
We have the following circuit on several boards and we have heating issues coming from the TPS40305.
With our current board configuration, only 1.8mA of output current is used on the…
Part Number: TPS40305 Hi, I would like to consult regarding assembly issue we had on TPS40305DRCR Boot capacitor (assembled between BOOT and SW pins). Mistakenly the assembled capacitor value was 1uF (instead of 100nF – as recommended on your datasheet…
Other Parts Discussed in Thread: TPS40305 I was successfully creating Webench designs with the TPS40305 on 10/14/16, but as of 10/15/16 every time I try to create a design - even the standard schematic from the product page - I get the message "Design cannot…
I was successfully creating Webench designs with the TPS40305 on 10/14/16, but as of 10/15/16 every time I try to create a design - even the standard schematic from the product page - I get the message "Design cannot be created with this device".…
Our design has the Vout connected to the FB pin (close to the TPS40305) though the datasheet's recommended RC network. Are there any issues in moving the Vout feedback point connection closer to the point of load? I am seeing too much drop in our…