Hi Ridge,
we are thinking of using TPS40140 for this application (even though it is an old part and no longer recommended by TI for new designs. Unfortunately the alternative suggested TPS40322 doesn't support the Vin range!). Does TPS40140 has any limitations…
Part Number: TPS40322 Dear ALL
Pls help to me .How to protection TPS40322 under test start up over voltage protection ?
Condition test is below .
1.Start up Over voltage protection test :
Condition test :Open feed back of TPS40322 then power on the…
Part Number: TPS40322 Other Parts Discussed in Thread: TPS53681 , TPS53647 Hi
How to use 2 x TPS40322 as Master and Slave (4 channels)?
These 2 pictures below are from datasheet. Apart from SYNC pin, what pin that I must connect between 2 x TPS40322.
…
Part Number: TPS40322 Hi E2E,
Could you kindly let us know how to calculate the resistor of remote sense? Is it simply Low-Pass filter?
If the resistor is too large, maybe 200~300k ohm (wrong component on PCB), Does VOUT will reach for OVP because RemSNS…
Part Number: TPS40322 Hi Team,
My customer want to use TPS40322 to do the Buck (Negative 3.8V~ Negative 2.8V), could you kindly recommended schematic for realizing this feature? Expect for your reply, thanks.
Best Regards
Benjamin
Part Number: TPS40322
Hi Experts,
Sorry for selecting wrong part number,the correct part number is TPS40322!
We encountered two phase non-balance isse at start-up, The one of phase would damaged caused by non-balance phenomenon
The one would operate BOOST…
Part Number: TPS40322 Hi E2E,
Our customer want to TI have the test to prove the EVM can PASS bode Plot as below conditions:
Phase margin > 50 degree
Gain margin < -20dB
Bandwidth range of 20%FSW~30% FSW
Could we have document about it?
If no…
Part Number: TPS40322 Hi E2E,
We use TPS40322 2-Phase solution and find VFB will from 0.6V rising to 0.606V when heavy load.
We also use fan to cool down the IC , but no any improve.
Did you have any idea to fix this issue?
Part Number: TPS40322 Hi E2E,
The datasheet describe as below:
Soft-star Cap CSS is 39nF, SS time = 2.34ms the 6 SS cycles is 14ms.
Why my hiccup time reach up to 31ms?
Part Number: TPS40322 Hi, Team:
Can you help to review TPS40322 schematic in attached file and give your comments? Working condition as below:
Vin : 12V ( typical )
Vout : 0.85V
Iout(max) : 40A
Vout ripple: 15mV
Vout overshoot: 25mV TPS40322 CORE POWER…