Part Number: TPS40322
Hi all,
Good day, i though i met something abnormal at EN1/SS1 pin,as figures below,is there anything that we should pay special attention to? thanks.
Can you help to review TPS40322 schematic and give your comments?thanks.
Vin …
Part Number: TPS40322 Hi, Team:
Can you help to review TPS40322 schematic in attached file and give your comments? Working condition as below:
Vin : 12V ( typical )
Vout : 0.85V
Iout(max) : 40A
Vout ripple: 15mV
Vout overshoot: 25mV TPS40322 CORE POWER…
Part Number: TPS40322 Hi,
We are using TPS40322. Found its PG will show noise during startup, as attached waveform Vout and PG. What is the potential reason that caused this kind of noise during Vout ramp up? Could you please help advise?
Thank you!
…
Part Number: TPS40322 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models Hello Team,
I change the TI TINA reference design of TPS40322 to single output as shown in TPS40322 datasheet Figure 29. Design Example 2, Two-Phase…
Part Number: TPS40322 Hello Team,
Via both TINA simulation of TPS40322 and measurement of EVM (single output version), EN pin max voltage is similar to BP6, 6V.
May we confirm if it is correct?
Thank you.
Regards,
Ting
Part Number: TPS40322 Other Parts Discussed in Thread: , PMP20516 Dear ALL
Pls help me , i need to know How to modify TPS40322EVM-074 to 5V/45A .
Bestregard
Prarinya
Part Number: TPS40322 Hello,
I use EN1/SS1 and EN2/SS2 separately on TPS40322 to sequence the power-up of my FPGA. I set 20 ms delay between each enable.
When I enable the CH1of the controller, VOUT1 (0.9 V) starts normally, but at the same time the VOUT2…
Part Number: TPS40322 Hi, team.
My customers have adapted TPS40322 in prototype, It is a situation that it can be using even in mass production prototype from now. (I have heard that no problem has arisen in particular.)
The other day, I was got a question…
Part Number: TPS40322 Regarding FB1, COMP1, COMP2, is figure 19 on page 17 an incomplete schematic with respect to the signals FB1, COMP1, COMP2? Does figure 19 current sharing pins CSx -/+ work with figure 18 pins FB1, COMP1, COMP2, DIFFO, ILIM and EN2…