Part Number: TPS40400 Other Parts Discussed in Thread: TPS40130 Tool/software: Hey Power Management team,
I have a customer working on a new project and we have a design challenge that we're hoping you can help provide guidance on.
We need to be able…
Part Number: TPS40400EVM-351 Other Parts Discussed in Thread: TPS40400 , USB-TO-GPIO2 , Hello!
Connect the TPS40400ENM-351 test board and adapter as shown in Figure 1, at the same time, apply 5V power to the input of the test board, then connect the…
Part Number: TPS40400 After the adapter was used for many times, it suddenly appeared abnormal. The software kept displaying no usb, and the adapter was very hot. Our use method is to connect the 10-pin terminal of the adapter to the product and the digital…
Part Number: TPS40400 I designed a tps40400.
But there is no output. Circuit is same with your webench.
BP3, BP6,VDD pin voltage is normal. There is no switching signal.
GUI status error is Vout OVF.
I don't know what's problem.
Part Number: TPS40400 Hi Expert,
My customer is using TPS40400 on one project. During the program burning procedure on the product line, they found one module couldn't import the input UVLO register value successfully. They checked the operation method…
Part Number: TPS40400 Other Parts Discussed in Thread: TMS320DM8168 Hi All,
We are using TPS40400 in our design for supplying AVS core supply to TMS320DM8168 processor. The address of the TPS40400 is programmed to 0x38(70 in octal) using resistors.…
Does TI have any plan to adapt TPS40400 driver to DVFS? Is it feasible or not?
Is there any side effect if we implement a frequent voltage change like DVFS on TPS40400?
Part Number: TPS40400 Hi Team,
during test on EVM, we find Vout reading through GUI is lower than voltage measure on Vsns+ - Vsns- . Please kindly see below.
test point on EVM : TP6 and TP18. TP6 and TP18 is connected directly to Vout and GND through…