Part Number: TPS40422 Other Parts Discussed in Thread: CSD87350Q5D , Hello,
My customer has a problem with the power MOSFET CSD87350Q5D used to build the TPS40422 circuitry being damaged in the field.
When only CSD87350Q5D was replaced, the same symptom…
Part Number: TPS40422 Other Parts Discussed in Thread: TPS40322 , can you share the TPS40422/TPS40322 DCR sense design workbook with me?
I have 12Vin 1.2Vo, 7.5A application, 1uH (4.2mohm DCR), 400khz fsw, want to use 0.1uF and 2.37K for DCR sense, pls…
Part Number: TPS40422 Hi Expert,
Customer would like to choose temperature sense transistor 2nd source of MMBT3904 which we used on the EVM. Could you please share what parameters should we consider when select the transistor?
Thanks.
Allan
Part Number: TPS40422 Hi TI Expert,
what's the status of SMB_ALERT status on TPS40422/25/28? is it open drain and need external pullp-up? i can't find the description from datasheet.
Thanks.
Part Number: TPS40422 For TPS40422, In Fusion GUI, XML files needs to be converted to CSV files. Could you please share the procedure for the same? Is there any method to do the conversion offline?
TPS40422
Part Number: TPS40422 Other Parts Discussed in Thread: CSD87350Q5D , TPS40322 Hi TI experts,
My customer has requested a SCH review for TPS 40422. For external fet, CSD87350Q5D was applied.
Attached the schematic and inductor datasheet.
xcu_power_sch.pd…
Part Number: TPS40422 Hi
PS: we set the per phase current limit 22A, so total current limit is 44A.
Why the Short Then On test the current is so match high(85A) than OCP and On Then Short test?
Why the negative voltage spike of -1.4V for ~60us, does…
Part Number: TPS40422 Hi Experts,
I have seen some documents that will define the pass criterion of the crossover frequency(Fco), for example, Fsw/30<Fco<Fsw/5. I want to know whether this pass criterion is necessary? In my result, both the gain margin…
Part Number: TPS40422 Customer would like to know about TPS40422, do we have default value for PMBUS page?
For example, when we read voltage value without writing into 'page', is it 'page 0' by default?