Part Number: TPS40425 Hi Sir
May you pls help double check TPS40425 circuit? because these some different between webench and datasheet.
Attached file is my customer circuit, May you pls also help check?
form now when i checking and now have some question…
Part Number: TPS40425 Hi
My Customer has question.
When the customer check the rising waveform, customer found an interesting point. Currently this waveform is not a problem, Will not you get advice on whether this waveform is working properly?
It is used…
Part Number: TPS40425 Hi
My customer has question.
The customer uses TPS40425 +CSD95378B in the 3 Phase circuit.
An alarm was raised with a current value lower than [OCW] [OCF] set during high load evaluation.
The customer is using [FUSION DIGITAL POWER…
Part Number: TPS40425 Other Parts Discussed in Thread: TPS40428 Hello
TPS40425 default is DCR sensing. If would like to change to Rds on sensing, which register of TPS40425 we can modify to Rds on sensing?
Below is schematics, if would…
Part Number: LM27403 Other Parts Discussed in Thread: CSD17573Q5B , , CSD17309Q3 , TPS40425 Hi Teams, In WEBENCH@ POWER DESIGNER, I select LM27403 (buck controller with discrete NMOSs) in DC/DC Power Designs. TPS40425 is a single phase controller combined…
Part Number: TPS40425 Other Parts Discussed in Thread: CSD95378BQ5M , , TPS53667 , TPS53647 Hello,
My customers are considering using the following specifications in the future.
They have questions about TPS40425 and CSD95378BQ5M.
Q: Do you have transient…
Part Number: TPS40425 Other Parts Discussed in Thread: TPS40428 , What is the maximum VOUT?
I have the same question with the TPS40428 should I repost?
Thanks
Part Number: TPS40425 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models I got Pspice transient model of TPS40425 from TI website and tried to build Macro in TINA but got error message; " Invalid device: $CDNENCSTART. Line…
Part Number: TPS40425 Hi
My Customer has question.
When running with 3 Phase, I think that it is necessary to set the value of
[IOUT_CAL_GAIN] to the same value as [Master IC] and [Slave IC].
Customer would like to set it in [Fusion Digital Power Designer…