Part Number: TPS40425EVM-594 Hi Sir
My customer use TPS40425 in 12Vin/0.8Vout 30A(2 phase one output) application.
May TPS40425 Turn on rise can be change by Fusion GUI? Because i change "Turn on Rise" and "Write to Hardware". but Vout rise time are all…
Part Number: TPS40425 Other Parts Discussed in Thread: TPS40140 Dear Sir
My customer want to survey 12V to 1V 300A solution,they have use TPS40425 and CSD95372A before.
Dose this solution can support 1V/300A applaction?
Part Number: TPS40425 Tool/software: WEBENCH® Design Tools Hi Sir
I have use webench to run Vin=12V/ Vout 3.3V/60A design. have some question as below:
1.i want to run the best optimize. but webench is shoe"Optimization data is not available for this…
Part Number: TPS40425 Other Parts Discussed in Thread: LM10011 , Hi
My customer has one question.Please cooperate.
customer are planning a use to C6678×2
Response to Smart Reflex will be TPS 40425 + LM10011×2 at Dual Phase.
Although TPS 40425…
Hi
My Customer has a question at datasheet P61 "E0h MFR_SPECIFIC_16 (COMM_EEPROM_SPARE)"
datasheet are written [15 bits] is at [Unused] .
Therefore,[15 bits] is either 1 and 0 ok?
Regards
T Kishi
Other Parts Discussed in Thread: TPS40425 Hi All,
Need the expert to help. I am trying to program the TPS40425 by using the command line.
It can scan the devices by using fusionpmbusscan and display the board total has 3 devices.
--> found device @ address…
Hi Nireeksha,
I typically recommend the 2xTPS543C20 or 2xTPS543C20A for the converter based 50A solution. Another option would utilize the 2xTPS546D24A.
Using a power module based solution (integrated inductors), I would recommend the 2xTPSM41625, TPSM831D31…
Other Parts Discussed in Thread: TPS53915 , TPS549B22 , TPS546A24A , TPS40400 , TPS40422 , TPS40425 Hi Team,
Could you pls suggest suitable parts for the requirements, thanks
(PWMs have PMBUS -- Vin 12V , Vout 1.0v 1.8v 3.3v MAX 3A)
Hi Tim,
RAMP is the triangle signal to eliminate the jitter. You can check the app. note below.
http://www.ti.com/lit/an/slua747a/slua747a.pdf
For 2phase controller with snackability, you may consider TPS40425/8.
Thanks
Chasel