Hello everybody,
does anybody have experiences operating the TPS43000-Controller (Multi-Top.) in Synchronous-Boost-Mode and Output Voltages
somewhat higher than 8V, means 8,4V?
Best regards
Frank
You are right. It is possible that the PFM at a different load level may alleviate the audible noise. Also I heard some engineers alter the capacitor and inductor orientations on the PCB such that the vibration is not reinforced among these parts. You…
Other Parts Discussed in Thread: TPS43000 I have a design using TPS43000 to create 15V output boost converter from two series li-Ion batteries in series. The output can supply up to about 10 amps for short periods. The circuit works well most of the time…
Other Parts Discussed in Thread: TPS43000 I am using for the first time the TPS43000 in Boost mode with 3V input for 5.5V out at 3.5 Amps output.
I am having problems getting over 1.2 amps output. My inductor is 2.2 uH, 7 Amp. Do I lower the resistor…
Hi,
1) i'm thinking to replace the voltage divider with a digital pot so that i can vary the output voltage with a microcontroller.
2) is there any other TI products that have simpler solution?
Any help is much appreciated, thank you.
Other Parts Discussed in Thread: TPS43000 How to use this controller as a bidirectional converter, for my application about hybrid storage system we need put two bidirectional controller for a Li-ion battery and for a Supercapacitor, I read a paper where…
Other Parts Discussed in Thread: TPS43000 Hi
Can you give me some information of how soft -start works for buck and Boost mode? on the TPS43000 controller, I just want to do a more precise simulation. please.
Greetings, I am in the process of building a boost circuit using the TPS 43000, schematic page 18 fig. 5, and are having a problem finding suitable power FETS, both n and p channel. The one's in the app. note Si9803DY and it's girlfriend Si9804DY are…