Part Number: TPS43060EVM-199 Other Parts Discussed in Thread: LM5122EVM-2PH , Can you provide the OrCAD DSN file of the TPS43060EVM-199 & LM5122EVM-2PH for project design?
Thanks.
Part Number: TPS43060EVM-199 Other Parts Discussed in Thread: TPS43060 I just received the eval board yesterday afternoon. I hook it up this morning with 18V/5A input power supply and 15 Ohms resistor and the circuit got stuck into some hiccup mode.
Part Number: TPS43060EVM-199 Other Parts Discussed in Thread: TPS43060 , Now TPS43060 does not work. The SS Pin only can reach 0.85V.
SS Pin of TPS43060 is always 0.47V. Even I short the SS pin with GND, it is still there after I remove the short jump…
Part Number: TPS43060EVM-199 I need a DC boost converter power source that will provide a constant 40VDC, but will pulse for signalling purposes at 32VDC. In other words, the circuit will operate at a nominal 40VDC - but will fluctuate down to 32VDC when…
Part Number: TPS43060EVM-199 Hi Team,
As title, could you please advise what needs to be modified on the TPS43060EVM-199 for a 12-24Vin, 54Vout/1.7A?
So far I found that the voltage rating of C2-C5 is too small.
Thanks!
Roy Hsu
Part Number: TPS43060EVM-199 Hello,
I am trying to determine the purpose of multiple vias on the input pad of boost inductor L1. Per layout figures 19, 20, 21, 22 of User's Guide (SLVU828A), these vias appear isolated on all underlying layers.
I would…
Other Parts Discussed in Thread: TPS43060EVM-199 Are the Gerber files available for the TPS43060EVM-199 evaluation module?
It may answer a few questions we have.
Thanks in advance.
Arthur Lekstutis
Part Number: TPS43060 Tool/software:
Hello, I would like to ask if there is an EMI test report for the TPS43060EVM-199 demo board? Because I saw in the document SLVU828A that this demo board does not follow the general universal layou method of DC-DC…
Part Number: TPS43060 Hello TI Team,
I am troubleshooting a radiated-noise problem on a board using the TPS43060RTER as a 15 V → 24 V boost converter (up to 2 A).
The system includes an 868 MHz RF transceiver, and the boost converter generates strong…
Part Number: TPS43061 Other Parts Discussed in Thread: TPS43060EVM-199 Hi Sir,
1. We use TPS43061 chip to design a dc-to-dc power, our input is 24Vdc, Output is 36V@3A, the schematic is the same TPS43060EVM-199. We use all the same components in our…