Part Number: TPS43061 Hi team,
My customer is trying to use TPS43061 and have 2 questions about the high side FET.
In general boost converter, normal diodes are used for high side rectification. But for this device, MOSFET are use for s ynchronous…
Part Number: TPS43061 Other Parts Discussed in Thread: LM5122 , Hi support team,
our customer consider for using muliti phase solution with TPS43061 like LM5122.
Looking the datasheet, It seems no problem to use it for multi phase because it has…
Part Number: TPS43061 Other Parts Discussed in Thread: TPS43060 , , CSD18543Q3A Hi,
I designed a circuit for the TPS43060 using webench to create a 36V 1A DC supply from a 6 to 8V DC input. The first articles worked fine, but TPS43060 is now out of…
Part Number: TPS43061 In the latest batch we've noticed that some TPS43061 devices on wake-up consume large currents from the VIN pin and do not functioning properly. The failure is intermittent (happens after multiple tries) and even when happens, the…
Part Number: TPS43061 Other Parts Discussed in Thread: CSD87350Q5D ,
I'm designing a 12V21.8A input 20V12.5A output 96% efficiency boost power supply, using the MOS for the CSD87350Q5D power block.
The design switching frequency is around 820kHz…
Hi lev,
Please let me know if you have further concerns. I'm still looking for the amplifier gain and slope comp info you asked for.
Thanks for considering TPS43061.
Part Number: TPS43061 Other Parts Discussed in Thread: CSD18543Q3A , Looking to find Mosfets which work well with Synchronous boost controller TPS43061. Would CSD18543Q3A be a good fit?
Part Number: TPS43061 Hi,
I am using TPS43061 in my project.
Vin : 12V to 16.4V
Vout : 36.5V
Peak Power : 360W
I face subharmonic oscillation at 14.4Vin and below when load at around 4A.
I wish to add external slope compensation circuit…
Part Number: TPS43061 Hi,
For TPS43061 external N-Ch MOSFET application requirement, we plan to use common FET ((SSM3K333R) as below diagram.
May I know is it OK to use this FET for our application?
The supply input Vin is from rechargeable battery…
Part Number: TPS43061 Other Parts Discussed in Thread: LMG5200 , I've been looking around for a synchronous boost control IC that might be suitable for driving the LMG5200, and it seems like the TPS43061 might be a good fit. My overall specifications…