Part Number: TPS43061 Other Parts Discussed in Thread: LM5155
Hoping you can give me a hint.
I used Webench and the TPS4306x design spreadsheet for guidance. I did what I think is a good layout (not my first switcher layout).
Switch node, current…
Part Number: TPS43061 Hi Team,
Our customer would like to cancel “ΔIL/2” of equation so they would like to take a limit at “Iave_max”.
Therefore, they add the capacitor to the following point.
Then, is there anything wrong?
Could you please…
Part Number: TPS43061 Other Parts Discussed in Thread: TPS43061 , TPS43060 please add a search box. forgive me if there is one.
I'm looking for every blog re TPS43061 . right now I'm reading every blog, to find tps43061. read 80 and I'm only back 7…
Part Number: TPS43061 Other Parts Discussed in Thread: TPS40210 , LM3478 , LM5155 , LM5156 , LM5122 We need a boost or buck-boost for Vin=9V or 12V and Vout=12V. The input voltage comes from USB-C port with PD support.
I expect TPS43061 to work as…
Part Number: TPS43061 Other Parts Discussed in Thread: TPS43060 I have a problem with the TPS43061. I had the circuit designed by webench (55V/2,5A). But the correct output voltage of 55V is only available at minimum load, as soon as the power is increased…
Part Number: TPS43061 Other Parts Discussed in Thread: LM5121 , Hello,
Can the top FET be reversed in a TPS43061RTER based regulator circuit to prevent the Vin from bleeding into Vout via the body diode?
Down stream of the TPS43061RTER, I am using…
Part Number: TPS43061 Other Parts Discussed in Thread: LM5121 Hello!
Now, I am testing the TPS43061 to boost input 5V to output 8V/3A.
When the EN is floating or pulled high, I get 8V output properly. However, the 4.7V output at load is still measured…
Part Number: TPS43061 Other Parts Discussed in Thread: TPS43060 Using Simetrix simulator TPS43061 SPICE Model (models, schematics available via email). But it gives error message (see image below) .
Also, as we are using SIMPLIS simulator for frequency…