Part Number: TPS4800-Q1 Tool/software: Hi,
TPS4800-Q1 datasheet doesn't have device marking information as below.
Let me know device marking to check components for SMT line.
Thank you.
Part Number: TPS4800-Q1 Tool/software: Hi,
I designed Back to Back Load switch using TPS4800-Q1 for 48V system.
When I test overvoltage case, I works well in case of cutoff response at rising(48V > 65V, Cutoff 58V) as like Figuire 8-10 in datasheet…
Part Number: TPS4800-Q1 Tool/software: Hi team,
I have one question on TPS4800-Q1.
The FLT_GD is described as UVLO of gate drive, why it is asserted when PU to SRC is above 7.5V, instead of below 7.5V?
BR,
Xiaoying
Part Number: TPS4800-Q1 Other Parts Discussed in Thread: TPS4810-Q1 Tool/software: Hi,
Q1. Please tell me the difference between TPS4800-Q1 and TPS4810-Q1.
Q2. These are preview versions, when will mass production be available?
Thanks,
Conor
Part Number: TPS4800-Q1 Tool/software: Hi,
I want to check the MOSFET SOA at the Short circuit protection case.
1. When I don't use C_TMR capacitor(only using resistor for pull-down), the short circuit protection response is fastest in datasheet. So…
Part Number: TPS4800-Q1
TPS4800 gives the possibility to measure the current via Vds-sensing
The datasheet does not give a hint what accuracy-levels can be expected when using this method vs. external shunt-measurement.
Of course the Vds-measurement…
Part Number: TPS4800-Q1 Hi TI team,
We are testing TPS4800-Q1 in our BMS application and we have the following observation.
Short circuit Latch OFF section is not working as expected.
After seeing short circuit set current, Vtmr started charging , MOSFET…
Part Number: TPS4800-Q1 Other Parts Discussed in Thread: TPS25948 , TPS2663 Hi,
do we have cost effective device for 5A high side switch for USB Type C - bi-directional power path?
BR
Max
Part Number: TPS1200-Q1 Is there any estimate you can provide for RTM for either of these parts? Looking forward to using them depending on the RTM schedule. Best
Dimitri