Part Number: TPS4810-Q1 I want to know the leakage current of TPS48100QDGXRQ1 in following conditons.
VIN range [ 40V ~ 54V ]
VEN = 0V
IC Tj range [ -40degC ~ 85degC]
Datasheet specifies 1uA as typical case and 4.6uA for worst case ( -40degC…
Part Number: TPS4810-Q1 In TPS4810, when the output is shorted SCP comparator only works when Vgs voltage is greater than 7V. But the Vgs of the FET used is only 3V. By the time SCP comparator works the currents are already very high, if the mosfets are…
Part Number: TPS4810-Q1 Other Parts Discussed in Thread: BQ76952 Hi TI Teams,
We are implementing the TPS4810 as a short-circuit protection solution for the charging path. In this design, the CHG pin of the BQ76952 is used to control the TPS4810.…
Part Number: TPS4810-Q1 Dear team,
My customer is evaluating TPS4810QDGXRQ1 but got a trouble. The customer nominal supply is 48V but it may beyond 100V in transient. Because of that, they consider to add TVS to protect it but still not 100% sure TVS…
Part Number: TPS4810-Q1 7.3.3 Short-Circuit Protection mentions I ISCP = 2 µA.
5.5 Electrical Characteristics lists I ISCP as ranging from 8.4 to 12.33 µA.
Please tell me which value is correct and the range.
Part Number: TPS4810-Q1 Hi expert,
My customer wants to know if the G1PU and G1PD and control the back-to-back MOSFET (Q1+Q2) at the same time? And use G2 float or control another MOSFET? Besides, can customer leaves G1PU, G1PD and G2 float of they…
Part Number: TPS4810-Q1 Dear team,
In case any failure, the voltage difference between Cs to Cs+ about >50V could be the reason of IC destruction? The time duration would be not too long.
Or negative voltage to Vs to Cs+ may cause the destruction…
Part Number: TPS4810-Q1 Tool/software: Is TPS4810-Q1 available ? Can you send me the cmp ds? I am looking to design it into our next rev motor drive design.